Hi Everyone,
I am using OMAP3530. I have two quiries
1. Is there any board in which OMAP3530 is used without TPS65950 & supporting SD card?
2. Can I use SD/MMC card with OMAP3530 without connecting SD/MMC card detection pin of SD/MMC connector to TPS65950 (P12 pin- GPIO0/ CD1)
& instead connect SD/MMC card detection pin of SD/MMC connector to some GPIO of OMAP3530.
Thanks in advance.
Regards,
Virun