OMAP-L138
OMAP-L138
The data sheet seems to be unclear on this point. Can anyone confirm?
For background, I submitted the following documentation feedback:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Adam,
Thanks for the suggestion. Would an update to section 5.34.3 be sufficient to clarify the confusion:
5.34.3 Initial Scan Chain Configuration
The first level of debug interface that sees the scan controller is the TAP router module. The debugger can configure the TAP router for serially linking up to 16 TAP controllers or individually scanning one of the TAP controllers without disrupting the IR state of the other TAPs. The TAP router also allows access to the Boundary Scan Architecture (please refer to BSDL (SPRM377b or SPRM376b) for more information.
Best Regards,
Erik