This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: Industrial-SDK ICSSG LWIP TCP server sample issue

Genius 3186 points
Part Number: PROCESSOR-SDK-AM64X


Hi 

May I have a question about tcpserver icssg example?

My customer and I testing enet on AM64x EVM (PROC101C).

And using ind_comms_sdk_am64x_09_00_00_03.

I could ping test on Enet Lwip ICSSG Example.

But on Enet Lwip TCP Server Example on ICSSG, we could not.

The log on manual, we could see IP address, but my log was not.

https://software-dl.ti.com/processor-industrial-sw/esd/ind_comms_sdk/am64x/09_00_00_03/docs/api_guide_am64x/EXAMPLES_ENET_LWIP_ICSSG_TCPSERVER.html 

I wrote down my log; 

DMSC Firmware Version 8.6.4--v08.06.04 (Chill Capybar
DMSC Firmware revision 0x8
DMSC ABI revision 3.1

INFO: Bootloader_runCpu:155: CPU r5f1-0  is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU m4f0-0 is initialized to 400000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU a530-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU a530-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:207: CPU r5f0-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runSelfCpu:217: All done, reseting self ...

==========================
ICSSG LWIP TCP ECHO SERVER
==========================
Enabling clocks!
Enabling clocks!
Mdio_open: MDIO Manual_Mode enabled
EnetPhy_bindDriver: PHY 15: OUI:080028 Model:0f Ver:01 <-> 'dp83869' : OK
PHY 3 is alive
PHY 15 is alive
Mdio_open: MDIO Manual_Mode enabled
EnetPhy_bindDriver: PHY 3: OUI:080028 Model:0f Ver:01 <-> 'dp83869' : OK
PHY 3 is alive
PHY 15 is alive
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 34:08:e1:80:b4:d0
[LWIPIF_LWIP] Enet has been started successfully
[0]Enet IF UP Event. Local interface IP:0.0.0.0
[LWIPIF_LWIP] NETIF INIT SUCCESS
EnetQueue_enq: NULL enq to the queue
Assertion @ Line: 111 in /nightlybuilds/mcupsdk_internal/jenkins/mcu_plus_sdk_am64x_09_00_00_35/source/networking/enet/core/src/core/enet_queue.c: node != NULL
                                                                               Icssg_handleLinkUp: icssg1-1: Port 1: Link up: 100-Mbps Full-Duplex

I think there is anything to EnetQueue_enq error.

If you notice anything, Could you let me know?

Thanks,

GR