This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDK 11, VS2 Demo Fail, Help~~~

Hello~~ the release of SDK 11 fail to run VS2 demo program.

My EVM is DDR2 REV.B. Using

SDK 11, uboot (for DDR2), KERNEL (VPSS & FB devices as module),

arago-base-tisdk-image-dm816x-evm.tar.gz as nfs fils system.

and run dm816x_sdk_05_00_00_11_vs_demo.zip.

------------------------------------------------------------------------------------------------

I' following the documents step to run demo program

mkdir /dev/syslinkipc/
 mknod /dev/syslinkipc/ProcMgr         c 254  0
 mknod /dev/syslinkipc/Notify          c 254  1
 mknod /dev/syslinkipc/NameServer      c 254  2
 mknod /dev/syslinkipc/SharedRegion    c 254  3
 mknod /dev/syslinkipc/HeapBufMP       c 254  4
 mknod /dev/syslinkipc/HeapMemMP       c 254  5
 mknod /dev/syslinkipc/HeapMultiBuf    c 254  6
 mknod /dev/syslinkipc/ListMP          c 254  7
 mknod /dev/syslinkipc/GateMP          c 254  8
 mknod /dev/syslinkipc/MessageQ        c 254  9
 mknod /dev/syslinkipc/MultiProc       c 254  10
 mknod /dev/syslinkipc/Ipc             c 254  11
 mknod /dev/syslinkipc/Osal            c 254  12
 mknod /dev/syslinkipc/SyslinkMemMgr   c 254  13
 mknod /dev/syslinkipc/ClientNotifyMgr c 254  14
 mknod /dev/syslinkipc/FrameQBufMgr    c 254  15
 mknod /dev/syslinkipc/FrameQ          c 254  16
 mknod /dev/syslinkipc/RingIO          c 254  17

# load module -----------------------------------
./prcm_config_app s;
insmod syslink.ko;
insmod TI81xx_HDMI.ko hdmi_mode=4;

./vs2_a8host_debug.xv5T

------------------------------------------------------------------------------------------------

I'm list my bootargs here:

bootargs=console=ttyO2,115200n8 noinitrd rw root=/dev/nfs nfsroot=192.168.1.238:/home/DVRTeam/jimmy/NVR_26XX/ti_demo/DM816x_SDK_05_00_00_11_VS_Demo/ti_nfs,nolock mem=256M earlyprintk vram=50M ip=192.168.3.181:::255.255.252.0::eth0:off

------------------------------------------------------------------------------------------------

The Error Message are


SDK VS Demo
===+=======
BUG: Your driver calls ioremap() on system memory.  This leads
<4>to architecturally unpredictable behaviour on ARMv6+, and ioremap()
<4>will fail in the next kernel release.  Please fix your driver.
------------[ cut here ]------------
WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0x58/0x190()
Modules linked in: TI81xx_hdmi syslink ipv6
Backtrace:
[<c0043b34>] (dump_backtrace+0x0/0x110) from [<c031afb8>] (dump_stack+0x18/0x1c)
 r7:00000000 r6:c00474c4 r5:c03c4ee1 r4:000000d3
[<c031afa0>] (dump_stack+0x0/0x1c) from [<c005b3e4>] (warn_slowpath_common+0x54/0x6c)
[<c005b390>] (warn_slowpath_common+0x0/0x6c) from [<c005b420>] (warn_slowpath_null+0x24/0x2c)
 r9:00000002 r8:00000001 r7:bf07b0a0 r6:00089000 r5:00060a68
r4:00000000
[<c005b3fc>] (warn_slowpath_null+0x0/0x2c) from [<c00474c4>] (__arm_ioremap_pfn_caller+0x58/0x190)
[<c004746c>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c0047680>] (__arm_ioremap_caller+0x64/0x6c)
[<c004761c>] (__arm_ioremap_caller+0x0/0x6c) from [<c0053d6c>] (omap_ioremap+0x60/0x64)
 r6:00000000 r5:00060a68 r4:89000000
[<c0053d0c>] (omap_ioremap+0x0/0x64) from [<bf07b0a0>] (MemoryOS_map+0x2ec/0x358 [syslink])
 r7:00000000 r6:00000005 r5:ccbf72ac r4:bf13b83c
[<bf07adb4>] (MemoryOS_map+0x0/0x358 [syslink]) from [<bf04d198>] (_ProcMgr_map+0x1fc/0x4c0 [syslink])
 r7:ccbf7310 r6:00000005 r5:ccbf7384 r4:d0bbd000
[<bf04cf9c>] (_ProcMgr_map+0x0/0x4c0 [syslink]) from [<bf05b370>] (ElfLoaderTrgWrite_copy+0x118/0x36c [syslink])
:

:

Can somebody help me ????

Best Regards - Jimmy