Part Number: LP-AM263
Hi,
I'm working on PRU-ICSS core of AM263x Launcpad. From the SDK Ver 9.0.0, I've got an example code of SENT encoder /decoder application, however there is minimal documentation for the same provided along with the example.
Also, for trying out this code, I would require two launchpad connected together.
Is there any working example supported for AM263x wherein we can configure GPIO in PRU core and get the data in R5 core, or similar examples which I can try out in the launchpad, with some good documentation?
Thanks,
Sreeraj