Other Parts Discussed in Thread: OMAP-L138
Hello, I am using OMAP-L138 EVM, and need to configure use USB ethernet. I configured the kernel as instructed in the PSP guide, but It results in problems with kernel startup. The messeges I get are: "sending DHCP requests .... timed out!" and then it tried again and again. What is the problem ? Did the ethernet moved automatically from the MII to the USB ? Should the ethernet cable be connected to the PC Host in order that the startup will continue normally ? Regards, Ran