Hi,
I have ported Android GingerBread 2.3.4 on Beagleboard-xM version.
Now i want to interface GSM modem with the board using the serial port.
From the schematic of beagleboard-xm(DM3730)
-- Uart 3 is coming on the board which cannot be used for interfacing(GSM modem) since it used for checking the boot parameters.
-- Uart 1 pins is a No Connect
-- Uart 2 pins are used for USB connections
can anyone help me out on how to interface the GSM modem using serial port without making any changes on the board
Regards
Prajith Warrier