This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 UART output



Hi all,

I am using DM368 Processor for video streaming process, i am facing the following problems which are listed below:

1. In UART mode, i am  getting the following output in my hyper terminal instead of the 'BOOTME' which usually comes as output from the DAVINCI when configured in UART mode

                                                                                       
P�tIG   �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P  P
�tIG    �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIg  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P
G       �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P
G       �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �P�tIG  �PI

 

2. Is NAND IC MT29F8G08ABABA compatible with DM368 ?

It will be really very helpful if someone can help in this.

Thanks

Varun