Other Parts Discussed in Thread: OMAP3530
Hi,
Conversion from YUV422 to YUV420SP is impossible though the resize function is mounted in ISP of OMAP3530.
Isn't there application processor or digital media processor that mounts the resize function that can be converted from YUV422 to YUV420SP?
DSP is not mounted and spec are inferior to OMAP3530 though it is possible to convert by the IPIPIE+RSZ function if it is DM36x.
Isn't there processor that mounts DSP in the ARM clock 1GHz class, and mounts the above-mentioned resize function?
Thanks in advvance for your cooperations.
Best regards,
yoshifumi