Q1:
Utilize generate_ DCC generated by dcc.sh_ 2a_ Wdr.bin and dcc_ Viss_ Wdr.bin file
When the camera is turned on, the image is very dark.
After investigation, it was found that this situation occurred when the. bin file was generated by adding the caf module.
What may be the reason for this?


Q2:
Different glbce strengths were used to generate the glbce.xml file.
It was found that there was no change in these two situations.
Is it because the file has not taken effect?