Other Parts Discussed in Thread: AM3517
Hi,
I want to set the CONFIG_MACH_FLASHBOARD to FALSE. Which files is located this define? I don't know where it is.
Thanks and Best Regards
Eric
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3517
Hi,
I want to set the CONFIG_MACH_FLASHBOARD to FALSE. Which files is located this define? I don't know where it is.
Thanks and Best Regards
Eric
Hi Eric,
You can disable flashboard from kernel menuconfig.
Location:
-> System Type
-> TI OMAP2/3/4 Specific Features
-> DM37X Flash Board
Disable DM37X Flash Board this will set CONFIG_MACH_FLASHBOARD to FALSE.
Regards,
Pankaj Bharadiya
Hi, Pankaj,
Thank you for your reply.
Actually, I want to port the LCD panel into Beagleboard. There are some control flag called CONFIG_MACH_FLASHBOARD. And then set it to FALSE. How to set it to FALSE?
Also I have one question. If I finish the selection of kernel menuconfig. I need to rebuild the uImage. I am using the following command to build the uImage:
Execute the following commands to the kernel sources
#> make ARCH=arm CROSS_COMPILE=arm-eabi- distclean
#> make ARCH=arm CROSS_COMPILE=arm-eabi- omap3_beagle_android_defconfig
Where default config is
omap3_evm_android_defconfig : For OMAP35x, AM37x, DM37x EVM
am3517_evm_android_defconfig : For AM35x EVM
omap3_beagle_android_defconfig : For Beagleboard Rev Cx, XM
#> make ARCH=arm CROSS_COMPILE=arm-eabi- uImage
Use this omap3_beagle_android_defconfig to build or other config define?
Thanks
Eric
If you need to customise your kernel image then your steps become:
1. $ make ARCH=arm CROSS_COMPILE=aem-eabi- distclean
2. $ make ARCH=arm CROSS_COMPILE=aem-eabi- omap3_beagle_android_defconfig
3. $ make ARCH=arm CROSS_COMPILE=aem-eabi- menuconfig
Here you can do your custom settings. Remember to save your kernel config after exiting the menuconfig.
4. make ARCH=arm CROSS_COMPILE=aem-eabi- uImage
In case you need to change the source code and Kconfig or Makefiles are modified, then perform steps 3 and 4 again.