Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: ADS7843, AM625, ADS7846
Hi TI,
we are using ADS7843 touch screen controller for our resistive touch LCD.
The Interrupt line of ADS7843 is connected to the one of the input port of IO expander.
on touch, the ADS7843 is interrupting the IO expander port as expected, how ever we see an error message on the debug console.
The message is as follows:
[ 1208.870828] ---[ end trace 3c8fa06a3e51791a ]---
[ 1404.961822] ------------[ cut here ]------------
[ 1404.966468] WARNING: CPU: 2 PID: 153 at drivers/gpio/gpiolib.c:2791 gpiod_get_raw_value+0x7c/0x98
[ 1404.975317] Modules linked in: md5 cbc crct10dif_ce pvrsrvkm(O) mcrc sa2ul sha512_generic authenc cryptodev(O)
[ 1404.985331] CPU: 2 PID: 153 Comm: irq/305-1-0022 Tainted: G W O 5.10.168-g2c23e6c538 #2
[ 1404.994440] Hardware name: Texas Instruments AM625 SK (DT)
[ 1404.999912] pstate: 20000005 (nzCv daif -PAN -UAO -TCO BTYPE=--)
[ 1405.005904] pc : gpiod_get_raw_value+0x7c/0x98
[ 1405.010334] lr : gpiod_get_raw_value+0x24/0x98
[ 1405.014763] sp : ffff80001215bc00
[ 1405.018065] x29: ffff80001215bc00 x28: ffff8000100bb000
[ 1405.023365] x27: ffff000001881c80 x26: ffff000001881c80
[ 1405.028665] x25: ffff0000017ead30 x24: 0000000000001ea5
[ 1405.033965] x23: ffff80001215bd48 x22: ffff0000018eb8dc
[ 1405.039264] x21: ffff0000018eb800 x20: 0000000000000000
[ 1405.044564] x19: ffff0000018f0a40 x18: ffff0000035e2800
[ 1405.049864] x17: 0000000000000000 x16: 0000000000000000
[ 1405.055165] x15: 000000523336af88 x14: 0000004b599ccb92
[ 1405.060464] x13: 0000000000000000 x12: 0000000000000001
[ 1405.065764] x11: 0000000000000062 x10: 00000000000009f0
[ 1405.071064] x9 : ffff80001215bac0 x8 : ffff00007fbb1e40
[ 1405.076363] x7 : ffff80006ebd7000 x6 : ffff00007fbb75c0
[ 1405.081662] x5 : 00000000410fd030 x4 : ffff8000111cfc88
[ 1405.086962] x3 : ffff00000039c800 x2 : ffff00000039c800
[ 1405.092261] x1 : 0000000000000001 x0 : ffff0000018f0220
[ 1405.097563] Call trace:
[ 1405.100001] gpiod_get_raw_value+0x7c/0x98
[ 1405.104089] get_pendown_state.isra.0.part.0+0x18/0x30
[ 1405.109213] ads7846_irq+0x310/0x418
[ 1405.112780] handle_nested_irq+0xb8/0x138
[ 1405.116781] pca953x_irq_handler+0x28c/0x308
[ 1405.121037] irq_thread_fn+0x2c/0xb0
[ 1405.124600] irq_thread+0x164/0x2e0
[ 1405.128080] kthread+0x140/0x160
[ 1405.131299] ret_from_fork+0x10/0x30
[ 1405.134864] ---[ end trace 3c8fa06a3e51791b ]---
[ 1405.149833] ------------[ cut here ]------------
[ 1405.154462] WARNING: CPU: 2 PID: 153 at drivers/gpio/gpiolib.c:2791 gpiod_get_raw_value+0x7c/0x98
[ 1405.163311] Modules linked in: md5 cbc crct10dif_ce pvrsrvkm(O) mcrc sa2ul sha512_generic authenc cryptodev(O)
[ 1405.173319] CPU: 2 PID: 153 Comm: irq/305-1-0022 Tainted: G W O 5.10.168-g2c23e6c538 #2
[ 1405.182428] Hardware name: Texas Instruments AM625 SK (DT)
[ 1405.187902] pstate: 20000005 (nzCv daif -PAN -UAO -TCO BTYPE=--)
[ 1405.193893] pc : gpiod_get_raw_value+0x7c/0x98
[ 1405.198323] lr : gpiod_get_raw_value+0x24/0x98
[ 1405.202752] sp : ffff80001215bc00
[ 1405.206054] x29: ffff80001215bc00 x28: ffff0000017eab68
[ 1405.211355] x27: 0000000000000fa0 x26: ffff000001881c80
[ 1405.216654] x25: ffff0000017ead30 x24: 0000000000001ea5
[ 1405.221954] x23: ffff0000018f1000 x22: ffff0000017eaca8
[ 1405.227253] x21: 0000000000000000 x20: 0000000000000001
[ 1405.232553] x19: ffff0000018f0a40 x18: 0000000033f989cf
[ 1405.237852] x17: 00000000b88bd8e6 x16: 00000000d7d91e46
[ 1405.243152] x15: 0000000000000000 x14: 0000000000000000
[ 1405.248451] x13: 0000000000000000 x12: 0000000000000049
[ 1405.253750] x11: 00000000000002c3 x10: 00000000000009f0
[ 1405.259050] x9 : ffff80001215bae0 x8 : ffff00007fbb1e40
[ 1405.264350] x7 : ffff80006ebd7000 x6 : ffff00007fbb75c0
[ 1405.269649] x5 : 00000000410fd030 x4 : ffff8000111cfc88
[ 1405.274949] x3 : ffff00000039c800 x2 : ffff00000039c800
[ 1405.280248] x1 : 0000000000000001 x0 : ffff0000018f0220
[ 1405.285548] Call trace:
[ 1405.287986] gpiod_get_raw_value+0x7c/0x98
[ 1405.292074] get_pendown_state.isra.0.part.0+0x18/0x30
[ 1405.297198] ads7846_irq+0x310/0x418
[ 1405.300765] handle_nested_irq+0xb8/0x138
[ 1405.304765] pca953x_irq_handler+0x28c/0x308
[ 1405.309022] irq_thread_fn+0x2c/0xb0
[ 1405.312585] irq_thread+0x164/0x2e0
[ 1405.316065] kthread+0x140/0x160
[ 1405.319285] ret_from_fork+0x10/0x30
[ 1405.322849] ---[ end trace 3c8fa06a3e51791c ]---
we are bit confused if its related to some conflict between touch screen controller and sha512_generic authenc cryptodev(O).
our dts configuration is as follows:
&main_spi2 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spitouch_pins_default>;
ti,pindir-d0-out-d1-in;
ads7843: ads7843@0 {
reg = <0>; /* CS0 */
compatible = "ti,ads7843";
interrupt-parent = <&exp1>;
interrupts = <12 IRQ_TYPE_EDGE_FALLING>; /* BOOT6 / GPIO 8 */
spi-max-frequency = <1000000>;
pendown-gpio = <&exp1 12 IRQ_TYPE_EDGE_FALLING>;
//vcc-supply = <&vcc_3v3_sys>;
ti,x-min = /bits/ 16 <0>;
ti,x-max = /bits/ 16 <8000>;
ti,y-min = /bits/ 16 <0>;
ti,y-max = /bits/ 16 <4800>;
ti,x-plate-ohms = /bits/ 16 <40>;
ti,pressure-max = /bits/ 16 <255>;
wakeup-source;
};
};
spitouch_pins_default: spitouch-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x01b0, PIN_OUTPUT_PULLUP, 1) /* (A20) MCASP0_ACLKR.SPI2_CLK */
AM62X_IOPAD(0x0194, PIN_OUTPUT_PULLUP, 1) /* (B19) MCASP0_AXR3.SPI2_D0 */
AM62X_IOPAD(0x0198, PIN_INPUT_PULLUP, 1) /* (A19) MCASP0_AXR2.SPI2_D1 */
AM62X_IOPAD(0x01ac, PIN_OUTPUT_PULLUP, 1) /* (E19) MCASP0_AFSR.SPI2_CS0 */
>;
};
Thanks and Regards,
Swapna