This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x ethernet

Hi,

The DM814x datasheet mentioned about an ethernet MAC switch.

It's not clear for me if it's possible to set up 2 independant ethernet interfaces, each having it's own MAC.

In our linux application the processor should act as a router, which means that the 2 ethernet interfaces may not be on a simple switch.

Is my fear correct that a single MAC is integrated?

 

Best Regards,

Wim

  • Wim,

    The DM814x Ethernet subsystem can be configured to appears as 2 individual Ethernet ports at the OS level.

    The hardware itself is capable of acting in this mode.

    Support for this mode of operation is currently planned for the September/October Linux PSP release.

     

    In this mode IP routing will be definitely possible between ports.

     

    Regards,

    Benoit

    P.S. If this response helps answer your question please mark this post as verified - Thanks!