This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build problem in shared region example of syslink

Other Parts Discussed in Thread: OMAP3530, SYSBIOS


Hi,

I am building shared region example of syslink for TI J4 platform.
I am using ezsdk_dm814x-evm_5_00_00_26_setuplinux.
I am able to build it for HLOS and facing problem at RTOS side.

making package.mak (because of package.bld) ...
ti.targets.C64P: warning: exec of '/u/users/TI_J4/ezsdk/cgt470_4_6_4/bin/cl6x --compiler_revision' failed:java.io.IOException: java.io.IOException: /u/users/TI_J4/ezsdk/cgt470_4_6_4/bin/cl6x: not found; check tools installation

generating interfaces for package ti.syslink.samples.rtos.notify (because package/package.xdc.inc is older than package.xdc) ...

configuring evm3530_dsp/whole_program_debug/notify_omap3530_dsp.x64P from package/cfg/evm3530_dsp/whole_program_debug/notify_omap3530_dsp_x64P.cfg ...

js: "./omap3530/Notify_omap3530_dsp.cfg", line 55: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'ti.sysbios.gates' along the path: '/u/users/TI_J4/ezsdk/ipc_1_22_03_23/packages/;/u/users/TI_J4/ezsdk/sysbios_6_31_04_27;/u/users/TI_J4/ezsdk/syslink_02_00_00_67/;/u/users/TI_J4/ezsdk/xdctools_3_20_07_86/packages;../../../../..;'. Ensure that the package path is set correctly.

    "./package/cfg/evm3530_dsp/whole_program_debug/notify_omap3530_dsp_x64P.cfg", line 787
    "./package/cfg/evm3530_dsp/whole_program_debug/notify_omap3530_dsp_x64P.cfg", line 842
    "./package/cfg/evm3530_dsp/whole_program_debug/notify_omap3530_dsp_x64P.cfg", line 774
gmake: *** [package/cfg/evm3530_dsp/whole_program_debug/notify_omap3530_dsp_x64P.xdl] Error 1


Could please help..




With Regards,
Ramakrishna.