This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: SBL boot failed

Genius 13655 points

Part Number: TDA4AL-Q1

Hello Champs,

 Customer used SBL mode and replaced the APP file with AutoSAR package.But the startup failed with the following log.

   However, AutoSAR packages can be run directly through the CCS debugger.

[17:54:41:475] SBL Revision: 01.00.10.01 (Sep 26 2023 - 19:30:50)␍␍␊
[17:54:41:698] TIFS ver: 8.6.3--v08.06.03 (Chill Capybar␍␍␊
[17:54:41:746] SCISERVER Board Configuration header population... PASSED␍␍␊
[17:54:41:810] Sciclient_setBoardConfigHeader... PASSED␍␍␊
[17:54:41:842] Initlialzing PLLs ...done.␍␍␊
[17:54:41:874] InitlialzingClocks ...done.␍␍␊
[17:54:41:906] Initlialzing DDR ...done.␍␍␊
[17:54:41:970] Initializing GTC ...Begin parsing user application␍␍␊
[17:54:42:018] Calling Sciclient_procBootRequestProcessor, ProcId 0x20... ␍␍␊
[17:54:42:082] Calling Sciclient_procBootRequestProcessor, ProcId 0x21... ␍␍␊
[17:54:42:146] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊
[17:54:42:210] Calling Sciclient_procBootRequestProcessor, ProcId 0x2... ␍␍␊
[17:54:42:273] Calling Sciclient_procBootRequestProcessor, ProcId 0x6... ␍␍␊
[17:54:42:321] Calling Sciclient_procBootRequestProcessor, ProcId 0x7... ␍␍␊
[17:54:42:385] Calling Sciclient_procBootRequestProcessor, ProcId 0x8... ␍␍␊
[17:54:42:449] Calling Sciclient_procBootRequestProcessor, ProcId 0x9... ␍␍␊
[17:54:42:513] Calling Sciclient_procBootRequestProcessor, ProcId 0x30... ␍␍␊
[17:54:42:561] Calling Sciclient_procBootRequestProcessor, ProcId 0x31... ␍␍␊
[17:54:42:625] Calling Sciclient_procBootRequestProcessor, ProcId 0x80... ␍␍␊
[17:54:42:769] Searching for X509 certificate ...found @0x41c7fb3c, size = 1746 bytes␍␍␍␊
[17:54:42:833] SBL reserved memory Found: Start = @ 0xc2000000, Size = 0x4000000␍␍␍␊
[17:54:42:912] Copying 1748 bytes from app to 0xc2000002␍␍␍␊
[17:54:42:960] Found seq @ 0xc200043d␍␍␍␊
[17:54:42:976] image length = 261428 bytes␍␍␍␊
[17:54:43:008] Copying 261432 bytes from offset 0x6d0 to 0xc20006d2...Cert @ 0xc2000002 ...Ignored on GP...done␍␍␍␊
[17:54:43:232] Switching core id 8, proc_id 0x1 to split mode... ␍␍␊
[17:54:43:280] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊
[17:54:43:344] Sciclient_procBootSetProcessorCfg, ProcId 0x1, enabling split mode...␍␍␊
[17:54:43:424] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊
[17:54:43:487] Enabling MCU TCMs after reset for core 8␍␍␊
[17:54:43:519] Disabling HW-based memory init of MCU TCMs for core 8␍␍␊
[17:54:43:583] Sciclient_procBootSetProcessorCfg update TCM enable/disable settings...␍␍␊
[17:54:43:647] Copying 0x40 bytes to 0x0␍␍␊
[17:54:43:679] Copying 0x444 bytes to 0x41cc0000␍␍␊
[17:54:43:711] Copying 0x314 bytes to 0x41cc1c44␍␍␊
[17:54:43:759] Copying 0x108 bytes to 0x41cc1f58␍␍␊
[17:54:43:791] Copying 0x8e8 bytes to 0x41cc2060␍␍␊
[17:54:43:823] Copying 0x11c44 bytes to 0x97000000␍␍␊
[17:54:43:855] Copying 0xd05c bytes to 0x97011c50␍␍␊
[17:54:43:903] Copying 0xbe6c bytes to 0x9701ecb0␍␍␊
[17:54:43:935] Copying 0x6134 bytes to 0x9702ab20␍␍␊
[17:54:43:967] Copying 0x45d4 bytes to 0x97035230␍␍␊
[17:54:44:015] Copying 0x41ac bytes to 0x97039804␍␍␊
[17:54:44:047] Copying 0x3fe8 bytes to 0x9703d9b0␍␍␊
[17:54:44:078] Copying 0x34 bytes to 0x970445a0␍␍␊
[17:54:44:110] Copying 0x8 bytes to 0x970445d4␍␍␊
[17:54:44:142] Copying 0x9e8 bytes to 0x97049450␍␍␊
[17:54:44:190] Copying 0x800 bytes to 0x9704a660␍␍␊
[17:54:44:222] Copying 0x458 bytes to 0x9704ae60␍␍␊
[17:54:44:254] Setting entry point for core 8 @0x41cc1f58␍␍␊
[17:54:44:302] Sciclient_procBootReleaseProcessor, ProcId 0x20...␍␍␊
[17:54:44:350] Sciclient_procBootReleaseProcessor, ProcId 0x21...␍␍␊
[17:54:44:398] Sciclient_procBootReleaseProcessor, ProcId 0x1...␍␍␊
[17:54:44:462] Sciclient_procBootReleaseProcessor, ProcId 0x2...␍␍␊
[17:54:44:510] Sciclient_procBootReleaseProcessor, ProcId 0x6...␍␍␊
[17:54:44:558] Sciclient_procBootReleaseProcessor, ProcId 0x7...␍␍␊
[17:54:44:606] Sciclient_procBootReleaseProcessor, ProcId 0x8...␍␍␊
[17:54:44:654] Sciclient_procBootReleaseProcessor, ProcId 0x9...␍␍␊
[17:54:44:717] Sciclient_procBootReleaseProcessor, ProcId 0x30...␍␍␊
[17:54:44:765] Sciclient_procBootReleaseProcessor, ProcId 0x31...␍␍␊
[17:54:44:813] Sciclient_procBootReleaseProcessor, ProcId 0x80...␍␍␊
[17:54:44:861] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊
[17:54:44:925] Sciclient_procBootSetProcessorCfg, ProcId 0x1, EntryPoint 0x41cc1f58...␍␍␊
[17:54:45:005] Sciclient_procBootSetProcessorCfg...FAILED


It related to

e2e.ti.com/.../tda4al-q1-sbl_slavecoreboot-failed-while-booting-entry-point-for-core-8-0x41cc1f58


Thanks
Regards
Shine