Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: AM625, AM62A7, DA8XX, PCF8575
Dear Ti experts:
when I want to boot from NAND .I encounterd a problem .
the message is below :U-Boot SPL 2021.01-00001-g45cb7e44ae-dirty (Oct 11 2023 - 18:45:22 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from NAND
then the uboot is stopped.
the sdk version: ti-processor-sdk-linux-am62xx-evm-08.06.00.42
the NAND :
MT29F4G08ABADAWP-IT:D/TSOP48 512M,2K of per page,128k per block.
the uboot r5_defconfig is below:
#
# Automatically generated file; DO NOT EDIT.
# U-Boot 2021.01 Configuration
#
#
# Compiler: arm-none-linux-gnueabihf-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025
#
CONFIG_CREATE_ARCH_SYMLINK=y
# CONFIG_ARC is not set
CONFIG_ARM=y
# CONFIG_M68K is not set
# CONFIG_MICROBLAZE is not set
# CONFIG_MIPS is not set
# CONFIG_NDS32 is not set
# CONFIG_NIOS2 is not set
# CONFIG_PPC is not set
# CONFIG_RISCV is not set
# CONFIG_SANDBOX is not set
# CONFIG_SH is not set
# CONFIG_X86 is not set
# CONFIG_XTENSA is not set
CONFIG_SYS_ARCH="arm"
CONFIG_SYS_CPU="armv7"
CONFIG_SYS_SOC="k3"
CONFIG_SYS_VENDOR="ti"
CONFIG_SYS_BOARD="am62x"
CONFIG_SYS_CONFIG_NAME="am62x_evm"
# CONFIG_SYS_ICACHE_OFF is not set
# CONFIG_SPL_SYS_ICACHE_OFF is not set
# CONFIG_SYS_DCACHE_OFF is not set
# CONFIG_SPL_SYS_DCACHE_OFF is not set
#
# ARM architecture
#
# CONFIG_GIC_V3_ITS is not set
CONFIG_HAS_THUMB2=y
CONFIG_ARM_ASM_UNIFIED=y
CONFIG_SYS_ARM_CACHE_CP15=y
# CONFIG_SYS_ARM_MMU is not set
CONFIG_SYS_ARM_MPU=y
CONFIG_CPU_V7R=y
CONFIG_SYS_ARM_ARCH=7
CONFIG_SYS_CACHE_SHIFT_6=y
CONFIG_SYS_CACHELINE_SIZE=64
CONFIG_SYS_ARM_CACHE_WRITEBACK=y
# CONFIG_SYS_ARM_CACHE_WRITETHROUGH is not set
# CONFIG_SYS_ARM_CACHE_WRITEALLOC is not set
# CONFIG_ARCH_CPU_INIT is not set
# CONFIG_SEMIHOSTING is not set
CONFIG_SYS_THUMB_BUILD=y
CONFIG_SPL_SYS_THUMB_BUILD=y
# CONFIG_SYS_L2CACHE_OFF is not set
# CONFIG_ENABLE_ARM_SOC_BOOT0_HOOK is not set
CONFIG_USE_ARCH_MEMCPY=y
CONFIG_SPL_USE_ARCH_MEMCPY=y
CONFIG_USE_ARCH_MEMSET=y
CONFIG_SPL_USE_ARCH_MEMSET=y
# CONFIG_ARCH_AT91 is not set
# CONFIG_TARGET_EDB93XX is not set
# CONFIG_TARGET_ASPENITE is not set
# CONFIG_TARGET_GPLUGD is not set
# CONFIG_ARCH_DAVINCI is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_MVEBU is not set
# CONFIG_TARGET_APF27 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_TARGET_SPEAR300 is not set
# CONFIG_TARGET_SPEAR310 is not set
# CONFIG_TARGET_SPEAR320 is not set
# CONFIG_TARGET_SPEAR600 is not set
# CONFIG_TARGET_STV0991 is not set
# CONFIG_TARGET_X600 is not set
# CONFIG_TARGET_FLEA3 is not set
# CONFIG_TARGET_MX35PDK is not set
# CONFIG_ARCH_BCM283X is not set
# CONFIG_ARCH_BCM63158 is not set
# CONFIG_ARCH_BCM68360 is not set
# CONFIG_ARCH_BCM6858 is not set
# CONFIG_TARGET_VEXPRESS_CA15_TC2 is not set
# CONFIG_ARCH_BCMSTB is not set
# CONFIG_TARGET_VEXPRESS_CA5X2 is not set
# CONFIG_TARGET_VEXPRESS_CA9X4 is not set
# CONFIG_TARGET_BCM23550_W1D is not set
# CONFIG_TARGET_BCM28155_AP is not set
# CONFIG_TARGET_BCMCYGNUS is not set
# CONFIG_TARGET_BCMNSP is not set
# CONFIG_TARGET_BCMNS2 is not set
# CONFIG_TARGET_BCMNS3 is not set
# CONFIG_ARCH_EXYNOS is not set
# CONFIG_ARCH_S5PC1XX is not set
# CONFIG_ARCH_HIGHBANK is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_IPQ40XX is not set
# CONFIG_ARCH_KEYSTONE is not set
CONFIG_ARCH_K3=y
# CONFIG_ARCH_OMAP2PLUS is not set
# CONFIG_ARCH_MESON is not set
# CONFIG_ARCH_MEDIATEK is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_IMX8 is not set
# CONFIG_ARCH_IMX8M is not set
# CONFIG_ARCH_IMXRT is not set
# CONFIG_ARCH_MX23 is not set
# CONFIG_ARCH_MX25 is not set
# CONFIG_ARCH_MX28 is not set
# CONFIG_ARCH_MX31 is not set
# CONFIG_ARCH_MX7ULP is not set
# CONFIG_ARCH_MX7 is not set
# CONFIG_ARCH_MX6 is not set
CONFIG_SPL_LDSCRIPT="arch/arm/mach-omap2/u-boot-spl.lds"
# CONFIG_ARCH_MX5 is not set
# CONFIG_ARCH_NEXELL is not set
# CONFIG_ARCH_OWL is not set
# CONFIG_ARCH_QEMU is not set
# CONFIG_ARCH_RMOBILE is not set
# CONFIG_TARGET_S32V234EVB is not set
# CONFIG_ARCH_SNAPDRAGON is not set
# CONFIG_ARCH_SOCFPGA is not set
# CONFIG_ARCH_SUNXI is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_VERSAL is not set
# CONFIG_ARCH_VF610 is not set
# CONFIG_ARCH_ZYNQ is not set
# CONFIG_ARCH_ZYNQMP_R5 is not set
# CONFIG_ARCH_ZYNQMP is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_TARGET_VEXPRESS64_AEMV8A is not set
# CONFIG_TARGET_VEXPRESS64_BASE_FVP is not set
# CONFIG_TARGET_VEXPRESS64_JUNO is not set
# CONFIG_TARGET_TOTAL_COMPUTE is not set
# CONFIG_TARGET_LS2080A_EMU is not set
# CONFIG_TARGET_LS2080A_SIMU is not set
# CONFIG_TARGET_LS1088AQDS is not set
# CONFIG_TARGET_LS2080AQDS is not set
# CONFIG_TARGET_LS2080ARDB is not set
# CONFIG_TARGET_LS2081ARDB is not set
# CONFIG_TARGET_LX2160ARDB is not set
# CONFIG_TARGET_LX2160AQDS is not set
# CONFIG_TARGET_LX2162AQDS is not set
# CONFIG_TARGET_HIKEY is not set
# CONFIG_TARGET_HIKEY960 is not set
# CONFIG_TARGET_POPLAR is not set
# CONFIG_TARGET_LS1012AQDS is not set
# CONFIG_TARGET_LS1012ARDB is not set
# CONFIG_TARGET_LS1012A2G5RDB is not set
# CONFIG_TARGET_LS1012AFRWY is not set
# CONFIG_TARGET_LS1012AFRDM is not set
# CONFIG_TARGET_LS1028AQDS is not set
# CONFIG_TARGET_LS1028ARDB is not set
# CONFIG_TARGET_LS1088ARDB is not set
# CONFIG_TARGET_LS1021AQDS is not set
# CONFIG_TARGET_LS1021ATWR is not set
# CONFIG_TARGET_LS1021ATSN is not set
# CONFIG_TARGET_LS1021AIOT is not set
# CONFIG_TARGET_LS1043AQDS is not set
# CONFIG_TARGET_LS1043ARDB is not set
# CONFIG_TARGET_LS1046AQDS is not set
# CONFIG_TARGET_LS1046ARDB is not set
# CONFIG_TARGET_LS1046AFRWY is not set
# CONFIG_TARGET_SL28 is not set
# CONFIG_TARGET_COLIBRI_PXA270 is not set
# CONFIG_ARCH_UNIPHIER is not set
# CONFIG_ARCH_STM32 is not set
# CONFIG_ARCH_STI is not set
# CONFIG_ARCH_STM32MP is not set
# CONFIG_ARCH_ROCKCHIP is not set
# CONFIG_ARCH_OCTEONTX is not set
# CONFIG_ARCH_OCTEONTX2 is not set
# CONFIG_TARGET_THUNDERX_88XX is not set
# CONFIG_ARCH_ASPEED is not set
# CONFIG_TARGET_DURIAN is not set
# CONFIG_TARGET_PRESIDIO_ASIC is not set
# CONFIG_TARGET_XENGUEST_ARM64 is not set
# CONFIG_TI_SECURE_DEVICE is not set
CONFIG_SYS_TEXT_BASE=0x80800000
CONFIG_TI_I2C_BOARD_DETECT=y
CONFIG_EEPROM_BUS_ADDRESS=0
CONFIG_EEPROM_CHIP_ADDRESS=0x50
# CONFIG_TI_COMMON_CMD_OPTIONS is not set
CONFIG_SPL_GPIO_SUPPORT=y
CONFIG_SPL_LIBCOMMON_SUPPORT=y
CONFIG_SPL_LIBGENERIC_SUPPORT=y
CONFIG_SYS_MALLOC_F_LEN=0x7000
CONFIG_NR_DRAM_BANKS=2
# CONFIG_SOC_K3_AM6 is not set
# CONFIG_SOC_K3_J721E is not set
# CONFIG_SOC_K3_J721S2 is not set
# CONFIG_SOC_K3_J784S4 is not set
# CONFIG_SOC_K3_AM642 is not set
CONFIG_SOC_K3_AM625=y
# CONFIG_SOC_K3_AM62A7 is not set
CONFIG_SYS_K3_NON_SECURE_MSRAM_SIZE=0x3c000
CONFIG_SYS_K3_MAX_DOWNLODABLE_IMAGE_SIZE=0x38000
CONFIG_SYS_K3_BOOT_PARAM_TABLE_INDEX=0x43c3f290
CONFIG_SYS_K3_KEY=""
CONFIG_SYS_K3_BOOT_CORE_ID=16
# CONFIG_K3_EARLY_CONS is not set
CONFIG_K3_LOAD_SYSFW=y
CONFIG_K3_SYSFW_IMAGE_NAME="sysfw.itb"
CONFIG_K3_SYSFW_IMAGE_MMCSD_RAW_MODE_SECT=0x3600
CONFIG_K3_SYSFW_IMAGE_SIZE_MAX=163840
CONFIG_K3_SYSFW_IMAGE_SPI_OFFS=0x6C0000
CONFIG_SYS_K3_SPL_ATF=y
CONFIG_K3_DM_FW=y
CONFIG_K3_ATF_LOAD_ADDR=0x70000000
CONFIG_K3_X509_SWRV=1
# CONFIG_TARGET_AM625_A53_EVM is not set
CONFIG_TARGET_AM625_R5_EVM=y
CONFIG_ENV_SIZE=0x20000
CONFIG_ENV_OFFSET=0x680000
CONFIG_DM_GPIO=y
# CONFIG_SPL_DM_SPI is not set
CONFIG_SPL_TEXT_BASE=0x43c00000
# CONFIG_SPL_MMC_SUPPORT is not set
CONFIG_SPL_SERIAL_SUPPORT=y
CONFIG_SPL_DRIVERS_MISC_SUPPORT=y
CONFIG_SPL_STACK_R_ADDR=0x82000000
CONFIG_SPL_SYS_MALLOC_F_LEN=0x7000
CONFIG_ERR_PTR_OFFSET=0x0
CONFIG_SPL_SIZE_LIMIT=0x3A7F0
CONFIG_SPL_SIZE_LIMIT_PROVIDE_STACK=0x3500
CONFIG_SPL=y
CONFIG_BOOTSTAGE_STASH_ADDR=0
CONFIG_IDENT_STRING=""
# CONFIG_SPL_FS_FAT is not set
CONFIG_SPL_LIBDISK_SUPPORT=y
# CONFIG_SPL_SPI_SUPPORT is not set
# CONFIG_CMD_DEKBLOB is not set
# CONFIG_CMD_HDMIDETECT is not set
CONFIG_IMX_DCD_ADDR=0x00910000
#
# ARM debug
#
# CONFIG_DEBUG_LL is not set
CONFIG_SPL_PAYLOAD="u-boot.bin"
CONFIG_BUILD_TARGET=""
CONFIG_DEFAULT_DEVICE_TREE="k3-am625-r5-sk"
# CONFIG_DEBUG_UART is not set
# CONFIG_AHCI is not set
# CONFIG_OF_BOARD_FIXUP is not set
#
# General setup
#
CONFIG_LOCALVERSION=""
CONFIG_LOCALVERSION_AUTO=y
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
# CONFIG_OPTIMIZE_INLINING is not set
# CONFIG_SPL_OPTIMIZE_INLINING is not set
CONFIG_CC_HAS_ASM_INLINE=y
# CONFIG_XEN is not set
# CONFIG_DISTRO_DEFAULTS is not set
# CONFIG_ENV_VARS_UBOOT_CONFIG is not set
# CONFIG_SYS_BOOT_GET_CMDLINE is not set
# CONFIG_SYS_BOOT_GET_KBD is not set
CONFIG_SYS_MALLOC_F=y
CONFIG_EXPERT=y
CONFIG_SYS_MALLOC_CLEAR_ON_INIT=y
# CONFIG_SYS_MALLOC_DEFAULT_TO_INIT is not set
# CONFIG_TOOLS_DEBUG is not set
# CONFIG_PHYS_64BIT is not set
CONFIG_SPL_IMAGE="spl/u-boot-spl.bin"
# CONFIG_SYS_CUSTOM_LDSCRIPT is not set
CONFIG_PLATFORM_ELFENTRY="_start"
CONFIG_STACK_SIZE=0x1000000
CONFIG_SYS_SRAM_BASE=0x0
CONFIG_SYS_SRAM_SIZE=0x0
# CONFIG_EXAMPLES is not set
#
# API
#
# CONFIG_API is not set
#
# Boot options
#
#
# Boot images
#
# CONFIG_ANDROID_BOOT_IMAGE is not set
CONFIG_FIT=y
CONFIG_FIT_EXTERNAL_OFFSET=0x0
CONFIG_FIT_ENABLE_SHA256_SUPPORT=y
# CONFIG_FIT_ENABLE_SHA384_SUPPORT is not set
# CONFIG_FIT_ENABLE_SHA512_SUPPORT is not set
# CONFIG_FIT_SIGNATURE is not set
# CONFIG_FIT_CIPHER is not set
# CONFIG_FIT_VERBOSE is not set
# CONFIG_FIT_BEST_MATCH is not set
CONFIG_SPL_FIT=y
# CONFIG_SPL_FIT_PRINT is not set
# CONFIG_SPL_FIT_SIGNATURE is not set
CONFIG_SPL_LOAD_FIT=y
CONFIG_SPL_LOAD_FIT_ADDRESS=0x80080000
# CONFIG_SPL_LOAD_FIT_APPLY_OVERLAY is not set
# CONFIG_SPL_LOAD_FIT_FULL is not set
CONFIG_SPL_FIT_IMAGE_POST_PROCESS=y
CONFIG_SPL_FIT_SOURCE=""
CONFIG_USE_SPL_FIT_GENERATOR=y
CONFIG_SPL_FIT_GENERATOR=""
CONFIG_LEGACY_IMAGE_FORMAT=y
# CONFIG_SUPPORT_RAW_INITRD is not set
# CONFIG_OF_BOARD_SETUP is not set
# CONFIG_OF_SYSTEM_SETUP is not set
# CONFIG_OF_STDOUT_VIA_ALIAS is not set
CONFIG_SYS_EXTRA_OPTIONS=""
CONFIG_HAVE_SYS_TEXT_BASE=y
CONFIG_ARCH_FIXUP_FDT_MEMORY=y
# CONFIG_CHROMEOS is not set
# CONFIG_CHROMEOS_VBOOT is not set
#
# Boot timing
#
# CONFIG_BOOTSTAGE is not set
CONFIG_BOOTSTAGE_RECORD_COUNT=30
CONFIG_SPL_BOOTSTAGE_RECORD_COUNT=5
CONFIG_TPL_BOOTSTAGE_RECORD_COUNT=5
CONFIG_BOOTSTAGE_STASH_SIZE=0x1000
# CONFIG_SHOW_BOOT_PROGRESS is not set
#
# Boot media
#
CONFIG_NAND_BOOT=y
# CONFIG_ONENAND_BOOT is not set
# CONFIG_QSPI_BOOT is not set
# CONFIG_SATA_BOOT is not set
# CONFIG_SD_BOOT is not set
# CONFIG_SPI_BOOT is not set
#
# Autoboot options
#
CONFIG_AUTOBOOT=y
CONFIG_BOOTDELAY=2
# CONFIG_AUTOBOOT_KEYED is not set
# CONFIG_AUTOBOOT_USE_MENUKEY is not set
# CONFIG_USE_BOOTARGS is not set
# CONFIG_USE_BOOTCOMMAND is not set
# CONFIG_USE_PREBOOT is not set
CONFIG_DEFAULT_FDT_FILE=""
#
# Console
#
# CONFIG_CONSOLE_RECORD is not set
# CONFIG_DISABLE_CONSOLE is not set
CONFIG_LOGLEVEL=4
CONFIG_SPL_LOGLEVEL=4
CONFIG_TPL_LOGLEVEL=4
# CONFIG_SILENT_CONSOLE is not set
# CONFIG_PRE_CONSOLE_BUFFER is not set
# CONFIG_CONSOLE_MUX is not set
# CONFIG_SYS_CONSOLE_IS_IN_ENV is not set
# CONFIG_SYS_CONSOLE_OVERWRITE_ROUTINE is not set
# CONFIG_SYS_CONSOLE_ENV_OVERWRITE is not set
# CONFIG_SYS_CONSOLE_INFO_QUIET is not set
# CONFIG_SYS_STDIO_DEREGISTER is not set
# CONFIG_SPL_SYS_STDIO_DEREGISTER is not set
# CONFIG_SYS_DEVICE_NULLDEV is not set
#
# Logging
#
# CONFIG_LOG is not set
#
# Init options
#
# CONFIG_BOARD_TYPES is not set
# CONFIG_DISPLAY_CPUINFO is not set
CONFIG_DISPLAY_BOARDINFO=y
# CONFIG_DISPLAY_BOARDINFO_LATE is not set
#
# Start-up hooks
#
# CONFIG_ARCH_EARLY_INIT_R is not set
# CONFIG_ARCH_MISC_INIT is not set
# CONFIG_BOARD_EARLY_INIT_F is not set
# CONFIG_BOARD_EARLY_INIT_R is not set
# CONFIG_BOARD_LATE_INIT is not set
# CONFIG_LAST_STAGE_INIT is not set
# CONFIG_MISC_INIT_R is not set
#
# Security support
#
CONFIG_HASH=y
#
# Update support
#
# CONFIG_UPDATE_TFTP is not set
# CONFIG_UPDATE_FIT is not set
# CONFIG_ANDROID_AB is not set
#
# Blob list
#
# CONFIG_BLOBLIST is not set
#
# SPL / TPL
#
CONFIG_SUPPORT_SPL=y
CONFIG_SPL_FRAMEWORK=y
# CONFIG_SPL_FRAMEWORK_BOARD_INIT_F is not set
CONFIG_SPL_SIZE_LIMIT_SUBTRACT_GD=y
CONFIG_SPL_SIZE_LIMIT_SUBTRACT_MALLOC=y
CONFIG_SPL_SYS_STACK_F_CHECK_BYTE=0xaa
CONFIG_SPL_SYS_REPORT_STACK_F_USAGE=y
#
# PowerPC and LayerScape SPL Boot options
#
CONFIG_SPL_BOARD_INIT=y
# CONFIG_SPL_BOOTROM_SUPPORT is not set
# CONFIG_SPL_BOOTCOUNT_LIMIT is not set
# CONFIG_SPL_RAW_IMAGE_SUPPORT is not set
# CONFIG_SPL_LEGACY_IMAGE_SUPPORT is not set
CONFIG_SPL_SYS_MALLOC_SIMPLE=y
CONFIG_SPL_STACK_R=y
CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN=0x100000
CONFIG_SPL_SEPARATE_BSS=y
CONFIG_SPL_BANNER_PRINT=y
CONFIG_SPL_EARLY_BSS=y
# CONFIG_SPL_DISPLAY_PRINT is not set
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR=y
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR=0x400
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_DATA_PART_OFFSET=0x0
# CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_PARTITION is not set
# CONFIG_SPL_CRC32_SUPPORT is not set
# CONFIG_SPL_MD5_SUPPORT is not set
# CONFIG_SPL_SHA1_SUPPORT is not set
# CONFIG_SPL_SHA256_SUPPORT is not set
# CONFIG_SPL_SHA384_SUPPORT is not set
# CONFIG_SPL_SHA512_SUPPORT is not set
# CONFIG_SPL_FIT_IMAGE_TINY is not set
# CONFIG_SPL_CACHE_SUPPORT is not set
# CONFIG_SPL_CPU_SUPPORT is not set
# CONFIG_SPL_CRYPTO_SUPPORT is not set
# CONFIG_SPL_HASH_SUPPORT is not set
CONFIG_SPL_DMA=y
CONFIG_SPL_ENV_SUPPORT=y
# CONFIG_SPL_SAVEENV is not set
# CONFIG_SPL_ETH_SUPPORT is not set
# CONFIG_SPL_FS_EXT4 is not set
# CONFIG_SPL_FS_SQUASHFS is not set
# CONFIG_SPL_FAT_WRITE is not set
# CONFIG_SPL_FPGA is not set
CONFIG_SPL_I2C_SUPPORT=y
CONFIG_SPL_DM_MAILBOX=y
CONFIG_SYS_MMCSD_FS_BOOT_PARTITION=1
# CONFIG_SPL_MPC8XXX_INIT_DDR_SUPPORT is not set
CONFIG_SPL_MTD_SUPPORT=y
# CONFIG_SPL_MTD_LOAD is not set
# CONFIG_SPL_MUSB_NEW_SUPPORT is not set
CONFIG_SPL_NAND_SUPPORT=y
CONFIG_SPL_NAND_DRIVERS=y
CONFIG_SPL_NAND_ECC=y
# CONFIG_SPL_NAND_SIMPLE is not set
CONFIG_SPL_NAND_BASE=y
CONFIG_SPL_NAND_IDENT=y
# CONFIG_SPL_UBI is not set
# CONFIG_SPL_DM_SPI_FLASH is not set
# CONFIG_SPL_NET_SUPPORT is not set
# CONFIG_SPL_NO_CPU_SUPPORT is not set
# CONFIG_SPL_NOR_SUPPORT is not set
# CONFIG_SPL_XIP_SUPPORT is not set
# CONFIG_SPL_ONENAND_SUPPORT is not set
# CONFIG_SPL_OS_BOOT is not set
# CONFIG_SPL_PCI is not set
# CONFIG_SPL_PCH_SUPPORT is not set
# CONFIG_SPL_POST_MEM_SUPPORT is not set
CONFIG_SPL_DM_RESET=y
# CONFIG_SPL_POWER_SUPPORT is not set
CONFIG_SPL_POWER_DOMAIN=y
# CONFIG_SPL_RAM_SUPPORT is not set
CONFIG_SPL_REMOTEPROC=y
# CONFIG_SPL_RTC_SUPPORT is not set
# CONFIG_SPL_SATA_SUPPORT is not set
# CONFIG_SPL_SPI_FLASH_MTD is not set
# CONFIG_SPL_THERMAL is not set
# CONFIG_SPL_USB_HOST_SUPPORT is not set
# CONFIG_SPL_USB_GADGET is not set
# CONFIG_SPL_WATCHDOG_SUPPORT is not set
# CONFIG_SPL_YMODEM_SUPPORT is not set
# CONFIG_SPL_AM33XX_ENABLE_RTC32K_OSC is not set
# CONFIG_SPL_OPTEE is not set
#
# Command line interface
#
CONFIG_CMDLINE=y
CONFIG_HUSH_PARSER=y
CONFIG_CMDLINE_EDITING=y
CONFIG_AUTO_COMPLETE=y
CONFIG_SYS_LONGHELP=y
CONFIG_SYS_PROMPT="=> "
CONFIG_SYS_XTRACE="y"
#
# Commands
#
#
# Info commands
#
# CONFIG_CMD_ACPI is not set
CONFIG_CMD_BDI=y
# CONFIG_CMD_CONFIG is not set
CONFIG_CMD_CONSOLE=y
# CONFIG_CMD_CPU is not set
# CONFIG_CMD_LICENSE is not set
# CONFIG_CMD_PMC is not set
#
# Boot commands
#
CONFIG_CMD_BOOTD=y
CONFIG_CMD_BOOTM=y
CONFIG_BOOTM_EFI=y
# CONFIG_CMD_BOOTZ is not set
CONFIG_BOOTM_LINUX=y
CONFIG_BOOTM_NETBSD=y
# CONFIG_BOOTM_OPENRTOS is not set
# CONFIG_BOOTM_OSE is not set
CONFIG_BOOTM_PLAN9=y
CONFIG_BOOTM_RTEMS=y
CONFIG_BOOTM_VXWORKS=y
CONFIG_CMD_BOOTEFI=y
CONFIG_CMD_BOOTEFI_HELLO_COMPILE=y
# CONFIG_CMD_BOOTEFI_HELLO is not set
# CONFIG_CMD_BOOTEFI_SELFTEST is not set
# CONFIG_CMD_BOOTMENU is not set
# CONFIG_CMD_ADTIMG is not set
CONFIG_CMD_ELF=y
CONFIG_CMD_FDT=y
CONFIG_CMD_GO=y
CONFIG_CMD_RUN=y
CONFIG_CMD_IMI=y
# CONFIG_CMD_IMLS is not set
CONFIG_CMD_XIMG=y
# CONFIG_CMD_SPL is not set
# CONFIG_CMD_THOR_DOWNLOAD is not set
# CONFIG_CMD_ZBOOT is not set
#
# Environment commands
#
CONFIG_CMD_ASKENV=y
CONFIG_CMD_EXPORTENV=y
CONFIG_CMD_IMPORTENV=y
CONFIG_CMD_EDITENV=y
# CONFIG_CMD_GREPENV is not set
CONFIG_CMD_SAVEENV=y
# CONFIG_CMD_ERASEENV is not set
CONFIG_CMD_ENV_EXISTS=y
# CONFIG_CMD_ENV_CALLBACK is not set
# CONFIG_CMD_ENV_FLAGS is not set
# CONFIG_CMD_NVEDIT_EFI is not set
# CONFIG_CMD_NVEDIT_INFO is not set
# CONFIG_CMD_NVEDIT_LOAD is not set
# CONFIG_CMD_NVEDIT_SELECT is not set
#
# Memory commands
#
# CONFIG_CMD_BINOP is not set
# CONFIG_CMD_BLOBLIST is not set
CONFIG_CMD_CRC32=y
# CONFIG_CRC32_VERIFY is not set
# CONFIG_CMD_EEPROM is not set
# CONFIG_LOOPW is not set
# CONFIG_CMD_MD5SUM is not set
# CONFIG_CMD_MEMINFO is not set
CONFIG_CMD_MEMORY=y
# CONFIG_CMD_MEM_SEARCH is not set
# CONFIG_CMD_MX_CYCLIC is not set
CONFIG_CMD_RANDOM=y
# CONFIG_CMD_MEMTEST is not set
# CONFIG_CMD_SHA1SUM is not set
# CONFIG_CMD_STRINGS is not set
#
# Compression commands
#
# CONFIG_CMD_LZMADEC is not set
# CONFIG_CMD_UNLZ4 is not set
# CONFIG_CMD_UNZIP is not set
# CONFIG_CMD_ZIP is not set
#
# Device access commands
#
# CONFIG_CMD_ARMFLASH is not set
# CONFIG_CMD_BCB is not set
# CONFIG_CMD_BIND is not set
# CONFIG_CMD_CLK is not set
# CONFIG_CMD_DEMO is not set
CONFIG_CMD_DFU=y
# CONFIG_CMD_DM is not set
CONFIG_CMD_FLASH=y
# CONFIG_CMD_FPGAD is not set
# CONFIG_CMD_FUSE is not set
# CONFIG_CMD_GPIO is not set
CONFIG_CMD_GPT=y
CONFIG_RANDOM_UUID=y
# CONFIG_CMD_GPT_RENAME is not set
# CONFIG_CMD_IDE is not set
# CONFIG_CMD_IO is not set
# CONFIG_CMD_IOTRACE is not set
# CONFIG_CMD_I2C is not set
CONFIG_CMD_LOADB=y
CONFIG_CMD_LOADS=y
# CONFIG_CMD_LSBLK is not set
# CONFIG_CMD_MISC is not set
CONFIG_CMD_MMC=y
# CONFIG_CMD_BKOPS_ENABLE is not set
# CONFIG_CMD_MMC_SWRITE is not set
# CONFIG_CMD_CLONE is not set
# CONFIG_CMD_MTD is not set
# CONFIG_CMD_NAND is not set
# CONFIG_CMD_ONENAND is not set
# CONFIG_CMD_OSD is not set
# CONFIG_CMD_PART is not set
# CONFIG_CMD_PCI is not set
CONFIG_CMD_PINMUX=y
# CONFIG_CMD_POWEROFF is not set
# CONFIG_CMD_READ is not set
CONFIG_CMD_REMOTEPROC=y
# CONFIG_CMD_SATA is not set
# CONFIG_CMD_SAVES is not set
# CONFIG_CMD_SCSI is not set
# CONFIG_CMD_SDRAM is not set
CONFIG_CMD_SF=y
# CONFIG_CMD_SF_TEST is not set
# CONFIG_CMD_SPI is not set
# CONFIG_CMD_TSI148 is not set
# CONFIG_CMD_UNIVERSE is not set
# CONFIG_CMD_USB is not set
# CONFIG_CMD_USB_SDP is not set
# CONFIG_CMD_USB_MASS_STORAGE is not set
#
# Shell scripting commands
#
CONFIG_CMD_ECHO=y
CONFIG_CMD_ITEST=y
CONFIG_CMD_SOURCE=y
# CONFIG_CMD_SETEXPR is not set
#
# Android support commands
#
#
# Misc commands
#
# CONFIG_CMD_BSP is not set
CONFIG_CMD_BLOCK_CACHE=y
# CONFIG_CMD_CACHE is not set
# CONFIG_CMD_CONITRACE is not set
# CONFIG_CMD_EFIDEBUG is not set
# CONFIG_CMD_EXCEPTION is not set
# CONFIG_CMD_DATE is not set
CONFIG_CMD_TIME=y
# CONFIG_CMD_GETTIME is not set
CONFIG_CMD_SLEEP=y
# CONFIG_MP is not set
# CONFIG_CMD_TIMER is not set
# CONFIG_CMD_SYSBOOT is not set
# CONFIG_CMD_QFW is not set
# CONFIG_CMD_PSTORE is not set
# CONFIG_CMD_TERMINAL is not set
# CONFIG_CMD_UUID is not set
#
# TI specific command line interface
#
# CONFIG_CMD_DDR3 is not set
# CONFIG_CMD_DDRSS is not set
# CONFIG_CMD_PD is not set
#
# Power commands
#
#
# Security commands
#
# CONFIG_CMD_AES is not set
# CONFIG_CMD_BLOB is not set
# CONFIG_CMD_HASH is not set
#
# Firmware commands
#
#
# Filesystem commands
#
# CONFIG_CMD_BTRFS is not set
# CONFIG_CMD_EXT2 is not set
# CONFIG_CMD_EXT4 is not set
CONFIG_CMD_FAT=y
# CONFIG_CMD_SQUASHFS is not set
# CONFIG_CMD_FS_GENERIC is not set
# CONFIG_CMD_FS_UUID is not set
# CONFIG_CMD_JFFS2 is not set
# CONFIG_CMD_MTDPARTS is not set
CONFIG_MTDIDS_DEFAULT=""
CONFIG_MTDPARTS_DEFAULT=""
# CONFIG_CMD_REISER is not set
# CONFIG_CMD_ZFS is not set
#
# Debug commands
#
# CONFIG_CMD_BEDBUG is not set
# CONFIG_CMD_DIAG is not set
# CONFIG_CMD_LOG is not set
# CONFIG_CMD_TRACE is not set
# CONFIG_CMD_UBI is not set
# CONFIG_MMC_SPEED_MODE_SET is not set
#
# Partition Types
#
CONFIG_PARTITIONS=y
# CONFIG_MAC_PARTITION is not set
# CONFIG_SPL_MAC_PARTITION is not set
CONFIG_DOS_PARTITION=y
CONFIG_SPL_DOS_PARTITION=y
# CONFIG_ISO_PARTITION is not set
# CONFIG_SPL_ISO_PARTITION is not set
# CONFIG_AMIGA_PARTITION is not set
# CONFIG_SPL_AMIGA_PARTITION is not set
CONFIG_EFI_PARTITION=y
CONFIG_EFI_PARTITION_ENTRIES_NUMBERS=128
CONFIG_EFI_PARTITION_ENTRIES_OFF=0
CONFIG_SPL_EFI_PARTITION=y
CONFIG_PARTITION_UUIDS=y
CONFIG_SPL_PARTITION_UUIDS=y
# CONFIG_PARTITION_TYPE_GUID is not set
CONFIG_SUPPORT_OF_CONTROL=y
CONFIG_DTC=y
#
# Device Tree Control
#
CONFIG_OF_CONTROL=y
CONFIG_SPL_OF_CONTROL=y
# CONFIG_OF_LIVE is not set
CONFIG_OF_SEPARATE=y
# CONFIG_OF_EMBED is not set
# CONFIG_OF_BOARD is not set
# CONFIG_OF_PRIOR_STAGE is not set
CONFIG_OF_LIST="k3-am625-r5-sk"
# CONFIG_MULTI_DTB_FIT is not set
CONFIG_SPL_MULTI_DTB_FIT=y
CONFIG_SPL_OF_LIST="k3-am625-r5-sk"
# CONFIG_SPL_MULTI_DTB_FIT_LZO is not set
# CONFIG_SPL_MULTI_DTB_FIT_GZIP is not set
CONFIG_SPL_MULTI_DTB_FIT_NO_COMPRESSION=y
CONFIG_OF_SPL_REMOVE_PROPS="interrupt-parent interrupts"
# CONFIG_OF_DTB_PROPS_REMOVE is not set
# CONFIG_SPL_OF_PLATDATA is not set
#
# Environment
#
CONFIG_ENV_SUPPORT=y
CONFIG_SAVEENV=y
# CONFIG_ENV_OVERWRITE is not set
# CONFIG_ENV_IS_NOWHERE is not set
# CONFIG_ENV_IS_IN_EEPROM is not set
# CONFIG_ENV_IS_IN_FAT is not set
# CONFIG_ENV_IS_IN_EXT4 is not set
# CONFIG_ENV_IS_IN_FLASH is not set
# CONFIG_ENV_IS_IN_MMC is not set
CONFIG_ENV_IS_IN_NAND=y
# CONFIG_ENV_IS_IN_NVRAM is not set
# CONFIG_ENV_IS_IN_ONENAND is not set
# CONFIG_ENV_IS_IN_REMOTE is not set
# CONFIG_ENV_IS_IN_SPI_FLASH is not set
# CONFIG_SYS_REDUNDAND_ENVIRONMENT is not set
# CONFIG_SYS_RELOC_GD_ENV_ADDR is not set
# CONFIG_USE_DEFAULT_ENV_FILE is not set
# CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG is not set
# CONFIG_ENV_APPEND is not set
# CONFIG_ENV_WRITEABLE_LIST is not set
# CONFIG_ENV_ACCESS_IGNORE_FORCE is not set
CONFIG_SPL_ENV_IS_NOWHERE=y
# CONFIG_VERSION_VARIABLE is not set
# CONFIG_NET is not set
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_DM=y
CONFIG_SPL_DM=y
CONFIG_DM_WARN=y
# CONFIG_SPL_DM_WARN is not set
# CONFIG_DM_DEBUG is not set
CONFIG_DM_DEVICE_REMOVE=y
# CONFIG_SPL_DM_DEVICE_REMOVE is not set
CONFIG_DM_STDIO=y
CONFIG_DM_SEQ_ALIAS=y
CONFIG_SPL_DM_SEQ_ALIAS=y
CONFIG_REGMAP=y
CONFIG_SPL_REGMAP=y
# CONFIG_SYSCON is not set
# CONFIG_SPL_SYSCON is not set
# CONFIG_DEVRES is not set
CONFIG_SIMPLE_BUS=y
CONFIG_SPL_SIMPLE_BUS=y
# CONFIG_SIMPLE_PM_BUS is not set
CONFIG_OF_TRANSLATE=y
CONFIG_SPL_OF_TRANSLATE=y
# CONFIG_TRANSLATION_OFFSET is not set
CONFIG_DM_DEV_READ_INLINE=y
# CONFIG_ACPIGEN is not set
# CONFIG_BOUNCE_BUFFER is not set
# CONFIG_ADC is not set
# CONFIG_ADC_EXYNOS is not set
# CONFIG_ADC_SANDBOX is not set
# CONFIG_SARADC_MESON is not set
# CONFIG_SARADC_ROCKCHIP is not set
# CONFIG_SATA is not set
# CONFIG_SCSI_AHCI is not set
#
# SATA/SCSI device support
#
# CONFIG_DWC_AHSATA is not set
# CONFIG_FSL_SATA is not set
# CONFIG_MVSATA_IDE is not set
# CONFIG_SATA_MV is not set
# CONFIG_SATA_SIL is not set
# CONFIG_SATA_SIL3114 is not set
# CONFIG_AXI is not set
#
# Bus devices
#
CONFIG_BLK=y
CONFIG_HAVE_BLOCK_DEVICE=y
CONFIG_SPL_BLK=y
CONFIG_BLOCK_CACHE=y
# CONFIG_SPL_BLOCK_CACHE is not set
# CONFIG_IDE is not set
# CONFIG_BOOTCOUNT_LIMIT is not set
#
# Button Support
#
# CONFIG_BUTTON is not set
#
# Cache Controller drivers
#
# CONFIG_CACHE is not set
# CONFIG_L2X0_CACHE is not set
# CONFIG_NCORE_CACHE is not set
#
# Clock
#
CONFIG_CLK=y
CONFIG_SPL_CLK=y
CONFIG_SPL_CLK_CCF=y
# CONFIG_SPL_CLK_COMPOSITE_CCF is not set
# CONFIG_CLK_CCF is not set
# CONFIG_CLK_TI_SCI is not set
# CONFIG_CLK_K3 is not set
CONFIG_SPL_CLK_K3=y
# CONFIG_CLK_K3_PLL is not set
CONFIG_SPL_CLK_K3_PLL=y
# CONFIG_CLK_CDCE9XX is not set
# CONFIG_CLK_AT91 is not set
# CONFIG_CLK_SIFIVE is not set
# CONFIG_ICS8N3QV01 is not set
# CONFIG_CLK_MPC83XX is not set
# CONFIG_CPU is not set
#
# Hardware crypto devices
#
# CONFIG_FSL_CAAM is not set
# CONFIG_SYS_FSL_SEC_BE is not set
# CONFIG_SYS_FSL_SEC_LE is not set
#
# Demo for driver model
#
# CONFIG_DM_DEMO is not set
#
# DFU support
#
CONFIG_DFU=y
# CONFIG_DFU_TFTP is not set
# CONFIG_DFU_TIMEOUT is not set
# CONFIG_DFU_MMC is not set
# CONFIG_DFU_RAM is not set
# CONFIG_DFU_SF is not set
# CONFIG_DFU_VIRT is not set
# CONFIG_SET_DFU_ALT_INFO is not set
CONFIG_SYS_DFU_DATA_BUF_SIZE=0x800000
CONFIG_SYS_DFU_MAX_FILE_SIZE=0x800000
#
# DMA Support
#
CONFIG_DMA=y
CONFIG_DMA_CHANNELS=y
# CONFIG_TI_EDMA3 is not set
CONFIG_TI_K3_NAVSS_UDMA=y
CONFIG_TI_K3_PSIL=y
#
# Fastboot support
#
CONFIG_FIRMWARE=y
CONFIG_SPL_FIRMWARE=y
CONFIG_TI_SCI_PROTOCOL=y
# CONFIG_ZYNQMP_FIRMWARE is not set
# CONFIG_SCMI_FIRMWARE is not set
#
# FPGA support
#
# CONFIG_FPGA_ALTERA is not set
# CONFIG_FPGA_SOCFPGA is not set
# CONFIG_FPGA_XILINX is not set
#
# GPIO Support
#
CONFIG_SPL_DM_GPIO=y
# CONFIG_GPIO_HOG is not set
# CONFIG_DM_GPIO_LOOKUP_LABEL is not set
# CONFIG_SPL_DM_GPIO_LOOKUP_LABEL is not set
# CONFIG_ALTERA_PIO is not set
# CONFIG_DWAPB_GPIO is not set
# CONFIG_AT91_GPIO is not set
# CONFIG_ATMEL_PIO4 is not set
CONFIG_DA8XX_GPIO=y
# CONFIG_INTEL_BROADWELL_GPIO is not set
# CONFIG_INTEL_GPIO is not set
# CONFIG_INTEL_ICH6_GPIO is not set
# CONFIG_IMX_RGPIO2P is not set
# CONFIG_IPROC_GPIO is not set
# CONFIG_HSDK_CREG_GPIO is not set
# CONFIG_LPC32XX_GPIO is not set
# CONFIG_MSM_GPIO is not set
# CONFIG_MXC_GPIO is not set
# CONFIG_MXS_GPIO is not set
# CONFIG_CMD_PCA953X is not set
# CONFIG_PCF8575_GPIO is not set
# CONFIG_ROCKCHIP_GPIO is not set
# CONFIG_XILINX_GPIO is not set
# CONFIG_CMD_TCA642X is not set
# CONFIG_TEGRA_GPIO is not set
# CONFIG_TEGRA186_GPIO is not set
# CONFIG_VYBRID_GPIO is not set
# CONFIG_SIFIVE_GPIO is not set
# CONFIG_ZYNQ_GPIO is not set
# CONFIG_DM_74X164 is not set
# CONFIG_DM_PCA953X is not set
# CONFIG_SPL_DM_PCA953X is not set
# CONFIG_MPC8XXX_GPIO is not set
# CONFIG_NX_GPIO is not set
#
# Hardware Spinlock Support
#
# CONFIG_DM_HWSPINLOCK is not set
#
# I2C support
#
CONFIG_DM_I2C=y
# CONFIG_I2C_SET_DEFAULT_BUS_NUM is not set
# CONFIG_DM_I2C_GPIO is not set
# CONFIG_SYS_I2C_IPROC is not set
# CONFIG_SYS_I2C_FSL is not set
# CONFIG_SYS_I2C_CADENCE is not set
# CONFIG_SYS_I2C_DW is not set
# CONFIG_SYS_I2C_INTEL is not set
# CONFIG_SYS_I2C_IMX_LPI2C is not set
# CONFIG_SYS_I2C_MXC is not set
# CONFIG_SYS_I2C_NEXELL is not set
# CONFIG_SYS_I2C_OCORES is not set
CONFIG_SYS_I2C_OMAP24XX=y
CONFIG_SYS_OMAP24_I2C_SLAVE=1
CONFIG_SYS_OMAP24_I2C_SPEED=100000
# CONFIG_SYS_I2C_ROCKCHIP is not set
# CONFIG_SYS_I2C_MVTWSI is not set
# CONFIG_SYS_I2C_XILINX_XIIC is not set
# CONFIG_SYS_I2C_IHS is not set
# CONFIG_I2C_MUX is not set
CONFIG_INPUT=y
# CONFIG_SPL_INPUT is not set
# CONFIG_DM_KEYBOARD is not set
# CONFIG_SPL_DM_KEYBOARD is not set
# CONFIG_CROS_EC_KEYB is not set
# CONFIG_TEGRA_KEYBOARD is not set
# CONFIG_TWL4030_INPUT is not set
#
# LED Support
#
# CONFIG_LED is not set
# CONFIG_SPL_LED is not set
# CONFIG_LED_STATUS is not set
#
# Mailbox Controller Support
#
CONFIG_DM_MAILBOX=y
CONFIG_K3_SEC_PROXY=y
#
# Memory Controller drivers
#
CONFIG_TI_GPMC=y
# CONFIG_TI_GPMC_DEBUG is not set
#
# Multifunction device drivers
#
CONFIG_MISC=y
# CONFIG_SPL_MISC is not set
# CONFIG_ALTERA_SYSID is not set
# CONFIG_ATSHA204A is not set
# CONFIG_ROCKCHIP_EFUSE is not set
# CONFIG_ROCKCHIP_OTP is not set
# CONFIG_SIFIVE_OTP is not set
# CONFIG_VEXPRESS_CONFIG is not set
# CONFIG_CROS_EC is not set
# CONFIG_SPL_CROS_EC is not set
# CONFIG_DS4510 is not set
# CONFIG_FSL_SEC_MON is not set
# CONFIG_NUVOTON_NCT6102D is not set
# CONFIG_PWRSEQ is not set
# CONFIG_PCA9551_LED is not set
# CONFIG_TWL4030_LED is not set
# CONFIG_WINBOND_W83627 is not set
# CONFIG_I2C_EEPROM is not set
# CONFIG_SPL_I2C_EEPROM is not set
# CONFIG_GDSYS_RXAUI_CTRL is not set
# CONFIG_GDSYS_IOEP is not set
# CONFIG_MPC83XX_SERDES is not set
# CONFIG_FS_LOADER is not set
# CONFIG_SPL_FS_LOADER is not set
# CONFIG_GDSYS_SOC is not set
# CONFIG_IHS_FPGA is not set
CONFIG_ESM_K3=y
# CONFIG_MICROCHIP_FLEXCOM is not set
#
# MMC Host controller Support
#
CONFIG_MMC=y
CONFIG_MMC_WRITE=y
# CONFIG_MMC_BROKEN_CD is not set
CONFIG_DM_MMC=y
CONFIG_SPL_DM_MMC=y
CONFIG_MMC_SDHCI_ADMA_HELPERS=y
# CONFIG_MMC_SPI is not set
# CONFIG_ARM_PL180_MMCI is not set
CONFIG_MMC_QUIRKS=y
CONFIG_MMC_HW_PARTITIONING=y
# CONFIG_SUPPORT_EMMC_RPMB is not set
# CONFIG_SUPPORT_EMMC_BOOT is not set
# CONFIG_MMC_IO_VOLTAGE is not set
# CONFIG_SPL_MMC_IO_VOLTAGE is not set
# CONFIG_MMC_HS400_ES_SUPPORT is not set
# CONFIG_SPL_MMC_HS400_ES_SUPPORT is not set
# CONFIG_MMC_HS400_SUPPORT is not set
# CONFIG_SPL_MMC_HS400_SUPPORT is not set
# CONFIG_MMC_HS200_SUPPORT is not set
CONFIG_SPL_MMC_HS200_SUPPORT=y
CONFIG_MMC_VERBOSE=y
# CONFIG_MMC_TRACE is not set
# CONFIG_MMC_DW is not set
# CONFIG_MMC_MXC is not set
# CONFIG_MMC_PCI is not set
# CONFIG_PXA_MMC_GENERIC is not set
# CONFIG_MMC_OMAP_HS is not set
CONFIG_MMC_SDHCI=y
CONFIG_MMC_SDHCI_IO_ACCESSORS=y
# CONFIG_MMC_SDHCI_SDMA is not set
CONFIG_MMC_SDHCI_ADMA=y
CONFIG_SPL_MMC_SDHCI_ADMA=y
# CONFIG_MMC_SDHCI_BCMSTB is not set
# CONFIG_MMC_SDHCI_CADENCE is not set
CONFIG_MMC_SDHCI_AM654=y
# CONFIG_MMC_SDHCI_IPROC is not set
# CONFIG_MMC_SDHCI_KONA is not set
# CONFIG_MMC_SDHCI_MSM is not set
# CONFIG_MMC_SDHCI_S5P is not set
# CONFIG_MMC_SDHCI_SPEAR is not set
# CONFIG_MMC_SDHCI_STI is not set
# CONFIG_MMC_SDHCI_XENON is not set
# CONFIG_MMC_SDHCI_TANGIER is not set
# CONFIG_MMC_SDHCI_ZYNQ is not set
# CONFIG_STM32_SDMMC2 is not set
# CONFIG_FTSDC010 is not set
# CONFIG_FSL_ESDHC is not set
# CONFIG_FSL_ESDHC_IMX is not set
#
# MTD Support
#
CONFIG_MTD=y
CONFIG_DM_MTD=y
# CONFIG_MTD_NOR_FLASH is not set
# CONFIG_SYS_MTDPARTS_RUNTIME is not set
# CONFIG_FLASH_CFI_DRIVER is not set
# CONFIG_CFI_FLASH is not set
# CONFIG_ALTERA_QSPI is not set
CONFIG_MTD_RAW_NAND=y
CONFIG_SYS_NAND_SELF_INIT=y
# CONFIG_SYS_NAND_USE_FLASH_BBT is not set
# CONFIG_NAND_ATMEL is not set
# CONFIG_NAND_BRCMNAND is not set
# CONFIG_NAND_DAVINCI is not set
# CONFIG_NAND_DENALI_DT is not set
# CONFIG_NAND_LPC32XX_SLC is not set
CONFIG_NAND_OMAP_GPMC=y
CONFIG_NAND_OMAP_GPMC_PREFETCH=y
CONFIG_NAND_OMAP_ELM=y
# CONFIG_NAND_VF610_NFC is not set
# CONFIG_NAND_PXA3XX is not set
# CONFIG_NAND_ARASAN is not set
# CONFIG_NAND_ZYNQ is not set
# CONFIG_NAND_OCTEONTX is not set
#
# Generic NAND options
#
# CONFIG_SYS_NAND_BUSWIDTH_16BIT is not set
# CONFIG_SYS_NAND_U_BOOT_LOCATIONS is not set
# CONFIG_SPL_NAND_AM33XX_BCH is not set
# CONFIG_SPL_NAND_DENALI is not set
# CONFIG_MTD_SPI_NAND is not set
#
# SPI Flash Support
#
CONFIG_DM_SPI_FLASH=y
CONFIG_SPI_FLASH=y
CONFIG_SF_DEFAULT_BUS=0
CONFIG_SF_DEFAULT_CS=0
CONFIG_SF_DEFAULT_MODE=0
CONFIG_SF_DEFAULT_SPEED=1000000
CONFIG_SPI_FLASH_SFDP_SUPPORT=y
CONFIG_SPI_FLASH_SMART_HWCAPS=y
CONFIG_SPI_FLASH_SOFT_RESET=y
CONFIG_SPI_FLASH_SOFT_RESET_ON_BOOT=y
# CONFIG_SPI_FLASH_BAR is not set
# CONFIG_SF_DUAL_FLASH is not set
# CONFIG_SPI_FLASH_ATMEL is not set
# CONFIG_SPI_FLASH_EON is not set
# CONFIG_SPI_FLASH_GIGADEVICE is not set
# CONFIG_SPI_FLASH_ISSI is not set
# CONFIG_SPI_FLASH_MACRONIX is not set
CONFIG_SPI_FLASH_SPANSION=y
CONFIG_SPI_FLASH_S28HS512T=y
CONFIG_SPI_FLASH_STMICRO=y
CONFIG_SPI_FLASH_MT35XU=y
# CONFIG_SPI_FLASH_SST is not set
# CONFIG_SPI_FLASH_WINBOND is not set
# CONFIG_SPI_FLASH_XMC is not set
CONFIG_SPI_FLASH_USE_4K_SECTORS=y
# CONFIG_SPI_FLASH_DATAFLASH is not set
# CONFIG_SPI_FLASH_MTD is not set
#
# UBI support
#
# CONFIG_UBI_SILENCE_MSG is not set
# CONFIG_MTD_UBI is not set
#
# Multiplexer drivers
#
# CONFIG_MULTIPLEXER is not set
# CONFIG_BITBANGMII is not set
# CONFIG_MV88E6352_SWITCH is not set
# CONFIG_FSL_PFE is not set
# CONFIG_DM_ETH is not set
# CONFIG_DM_ETH_PHY is not set
# CONFIG_PCI is not set
#
# PCI Endpoint
#
# CONFIG_PCI_ENDPOINT is not set
# CONFIG_X86_PCH7 is not set
# CONFIG_X86_PCH9 is not set
#
# PHY Subsystem
#
# CONFIG_PHY is not set
# CONFIG_SPL_PHY is not set
#
# Rockchip PHY driver
#
# CONFIG_PHY_CADENCE_SIERRA is not set
# CONFIG_PHY_CADENCE_TORRENT is not set
# CONFIG_PHY_J721E_WIZ is not set
# CONFIG_MVEBU_COMPHY_SUPPORT is not set
#
# Pin controllers
#
CONFIG_PINCTRL=y
CONFIG_PINCTRL_FULL=y
# CONFIG_PINCTRL_GENERIC is not set
CONFIG_PINCONF_RECURSIVE=y
CONFIG_SPL_PINCTRL=y
CONFIG_SPL_PINCTRL_FULL=y
# CONFIG_SPL_PINCTRL_GENERIC is not set
CONFIG_SPL_PINCONF_RECURSIVE=y
# CONFIG_PINCTRL_AT91 is not set
# CONFIG_PINCTRL_AT91PIO4 is not set
# CONFIG_PINCTRL_INTEL is not set
# CONFIG_PINCTRL_QE is not set
# CONFIG_PINCTRL_ROCKCHIP_RV1108 is not set
CONFIG_PINCTRL_SINGLE=y
# CONFIG_PINCTRL_STM32 is not set
# CONFIG_PINCTRL_STMFX is not set
# CONFIG_SPL_PINCTRL_STMFX is not set
#
# Power
#
# CONFIG_ACPI_PMC is not set
# CONFIG_SPL_ACPI_PMC is not set
# CONFIG_TPL_ACPI_PMC is not set
#
# Power Domain Support
#
CONFIG_POWER_DOMAIN=y
# CONFIG_TI_SCI_POWER_DOMAIN is not set
CONFIG_TI_POWER_DOMAIN=y
# CONFIG_DM_PMIC is not set
# CONFIG_PMIC_AS3722 is not set
# CONFIG_POWER_MC34VR500 is not set
# CONFIG_DM_REGULATOR is not set
# CONFIG_POWER_MT6323 is not set
# CONFIG_DM_PWM is not set
# CONFIG_PWM_IMX is not set
# CONFIG_PWM_SANDBOX is not set
# CONFIG_U_QE is not set
CONFIG_RAM=y
CONFIG_SPL_RAM=y
# CONFIG_TPL_RAM is not set
# CONFIG_STM32_SDRAM is not set
# CONFIG_MPC83XX_SDRAM is not set
CONFIG_K3_DDRSS=y
# CONFIG_K3_J721E_DDRSS is not set
# CONFIG_K3_J721S2_DDRSS is not set
# CONFIG_K3_J784S4_DDRSS is not set
CONFIG_K3_AM64_DDRSS=y
# CONFIG_K3_AM62A_DDRSS is not set
# CONFIG_IMXRT_SDRAM is not set
# CONFIG_ROCKCHIP_SDRAM_COMMON is not set
#
# Remote Processor drivers
#
CONFIG_REMOTEPROC=y
CONFIG_K3_SYSTEM_CONTROLLER=y
CONFIG_REMOTEPROC_TI_K3_ARM64=y
# CONFIG_REMOTEPROC_TI_K3_DSP is not set
# CONFIG_REMOTEPROC_TI_K3_R5F is not set
# CONFIG_REMOTEPROC_TI_K3_M4F is not set
#
# Reset Controller Support
#
CONFIG_DM_RESET=y
CONFIG_RESET_TI_SCI=y
# CONFIG_RESET_AST2500 is not set
# CONFIG_RESET_HISILICON is not set
# CONFIG_RESET_SYSCON is not set
# CONFIG_RESET_SCMI is not set
# CONFIG_RESET_DRA7 is not set
# CONFIG_DM_RNG is not set
#
# Real Time Clock
#
# CONFIG_DM_RTC is not set
# CONFIG_SPL_DM_RTC is not set
# CONFIG_RTC_ENABLE_32KHZ_OUTPUT is not set
# CONFIG_RTC_PCF8563 is not set
# CONFIG_RTC_RX8025 is not set
# CONFIG_RTC_PL031 is not set
# CONFIG_RTC_S35392A is not set
# CONFIG_RTC_MC146818 is not set
# CONFIG_RTC_M41T62 is not set
# CONFIG_SCSI is not set
# CONFIG_DM_SCSI is not set
#
# Serial drivers
#
CONFIG_BAUDRATE=115200
CONFIG_REQUIRE_SERIAL_CONSOLE=y
CONFIG_SPECIFY_CONSOLE_INDEX=y
CONFIG_SERIAL_PRESENT=y
CONFIG_SPL_SERIAL_PRESENT=y
CONFIG_CONS_INDEX=1
CONFIG_DM_SERIAL=y
# CONFIG_SERIAL_RX_BUFFER is not set
# CONFIG_SERIAL_SEARCH_ALL is not set
CONFIG_SPL_DM_SERIAL=y
# CONFIG_ALTERA_JTAG_UART is not set
# CONFIG_ALTERA_UART is not set
# CONFIG_ARC_SERIAL is not set
# CONFIG_ARM_DCC is not set
# CONFIG_ATMEL_USART is not set
# CONFIG_BCM6345_SERIAL is not set
# CONFIG_COREBOOT_SERIAL is not set
# CONFIG_CORTINA_UART is not set
# CONFIG_FSL_LINFLEXUART is not set
# CONFIG_FSL_LPUART is not set
# CONFIG_MVEBU_A3700_UART is not set
# CONFIG_MCFUART is not set
# CONFIG_NULLDEV_SERIAL is not set
CONFIG_SYS_NS16550=y
# CONFIG_NS16550_DYNAMIC is not set
# CONFIG_PL01X_SERIAL is not set
# CONFIG_XILINX_UARTLITE is not set
# CONFIG_MSM_SERIAL is not set
CONFIG_OMAP_SERIAL=y
# CONFIG_PXA_SERIAL is not set
# CONFIG_SIFIVE_SERIAL is not set
# CONFIG_ZYNQ_SERIAL is not set
# CONFIG_MTK_SERIAL is not set
# CONFIG_SMEM is not set
#
# Sound support
#
# CONFIG_SOUND is not set
#
# SOC (System On Chip) specific Drivers
#
CONFIG_SOC_DEVICE=y
CONFIG_SOC_DEVICE_TI_K3=y
CONFIG_SOC_TI=y
CONFIG_TI_K3_NAVSS_RINGACC=y
CONFIG_SPI=y
CONFIG_DM_SPI=y
CONFIG_SPI_MEM=y
# CONFIG_ALTERA_SPI is not set
# CONFIG_ATCSPI200_SPI is not set
# CONFIG_ATMEL_SPI is not set
# CONFIG_BCMSTB_SPI is not set
# CONFIG_CORTINA_SFLASH is not set
CONFIG_CADENCE_QSPI=y
# CONFIG_CF_SPI is not set
# CONFIG_DESIGNWARE_SPI is not set
# CONFIG_EXYNOS_SPI is not set
# CONFIG_FSL_DSPI is not set
# CONFIG_FSL_QSPI is not set
# CONFIG_ICH_SPI is not set
# CONFIG_KIRKWOOD_SPI is not set
# CONFIG_MPC8XXX_SPI is not set
# CONFIG_MTK_SNFI_SPI is not set
# CONFIG_MVEBU_A3700_SPI is not set
# CONFIG_MXS_SPI is not set
# CONFIG_NXP_FSPI is not set
# CONFIG_OMAP3_SPI is not set
# CONFIG_PL022_SPI is not set
# CONFIG_ROCKCHIP_SPI is not set
# CONFIG_SPI_SIFIVE is not set
# CONFIG_SOFT_SPI is not set
# CONFIG_SPI_SUNXI is not set
# CONFIG_TEGRA114_SPI is not set
# CONFIG_TEGRA20_SFLASH is not set
# CONFIG_TEGRA20_SLINK is not set
# CONFIG_TEGRA210_QSPI is not set
# CONFIG_TI_QSPI is not set
# CONFIG_XILINX_SPI is not set
# CONFIG_ZYNQ_SPI is not set
# CONFIG_ZYNQ_QSPI is not set
# CONFIG_ZYNQMP_GQSPI is not set
# CONFIG_FSL_ESPI is not set
# CONFIG_SH_QSPI is not set
# CONFIG_MXC_SPI is not set
#
# SPMI support
#
# CONFIG_SPMI is not set
# CONFIG_SYSINFO is not set
#
# System reset device drivers
#
# CONFIG_SYSRESET is not set
# CONFIG_SYSRESET_SYSCON is not set
# CONFIG_SYSRESET_WATCHDOG is not set
# CONFIG_SYSRESET_RESETCTL is not set
# CONFIG_SYSRESET_MPC83XX is not set
# CONFIG_OPTEE is not set
# CONFIG_DM_THERMAL is not set
#
# Timer Support
#
CONFIG_TIMER=y
CONFIG_SPL_TIMER=y
# CONFIG_TIMER_EARLY is not set
# CONFIG_ALTERA_TIMER is not set
# CONFIG_AST_TIMER is not set
# CONFIG_ATCPIT100_TIMER is not set
# CONFIG_ATMEL_PIT_TIMER is not set
# CONFIG_CADENCE_TTC_TIMER is not set
# CONFIG_DESIGNWARE_APB_TIMER is not set
# CONFIG_MPC83XX_TIMER is not set
# CONFIG_RENESAS_OSTM_TIMER is not set
# CONFIG_NOMADIK_MTU_TIMER is not set
CONFIG_OMAP_TIMER=y
# CONFIG_ROCKCHIP_TIMER is not set
# CONFIG_STI_TIMER is not set
# CONFIG_STM32_TIMER is not set
# CONFIG_MTK_TIMER is not set
# CONFIG_MCHP_PIT64B_TIMER is not set
#
# TPM support
#
# CONFIG_USB is not set
#
# UFS Host Controller Support
#
# CONFIG_TI_J721E_UFS is not set
#
# Graphics support
#
# CONFIG_DM_VIDEO is not set
# CONFIG_SYS_WHITE_ON_BLACK is not set
# CONFIG_NO_FB_CLEAR is not set
#
# TrueType Fonts
#
# CONFIG_VIDEO_VESA is not set
# CONFIG_VIDEO_LCD_ANX9804 is not set
# CONFIG_VIDEO_LCD_SSD2828 is not set
# CONFIG_VIDEO_MVEBU is not set
# CONFIG_I2C_EDID is not set
# CONFIG_DISPLAY is not set
# CONFIG_ATMEL_HLCD is not set
# CONFIG_AM335X_LCD is not set
# CONFIG_VIDEO_TEGRA20 is not set
# CONFIG_VIDEO_BRIDGE is not set
# CONFIG_VIDEO is not set
# CONFIG_LCD is not set
# CONFIG_VIDEO_SIMPLE is not set
# CONFIG_VIDEO_DT_SIMPLEFB is not set
# CONFIG_OSD is not set
# CONFIG_SPLASH_SCREEN is not set
# CONFIG_VIDEO_VCXK is not set
#
# VirtIO Drivers
#
# CONFIG_VIRTIO_MMIO is not set
#
# 1-Wire support
#
# CONFIG_W1 is not set
#
# 1-wire EEPROM support
#
# CONFIG_W1_EEPROM is not set
#
# Watchdog Timer Support
#
# CONFIG_WATCHDOG is not set
CONFIG_WATCHDOG_TIMEOUT_MSECS=60000
# CONFIG_IMX_WATCHDOG is not set
# CONFIG_ULP_WATCHDOG is not set
# CONFIG_DESIGNWARE_WATCHDOG is not set
# CONFIG_WDT is not set
# CONFIG_SPL_WDT is not set
# CONFIG_PVBLOCK is not set
# CONFIG_PHYS_TO_BUS is not set
#
# File systems
#
# CONFIG_FS_BTRFS is not set
# CONFIG_FS_CBFS is not set
# CONFIG_SPL_FS_CBFS is not set
# CONFIG_FS_EXT4 is not set
CONFIG_FS_FAT=y
CONFIG_FAT_WRITE=y
CONFIG_FS_FAT_MAX_CLUSTSIZE=65536
# CONFIG_FS_JFFS2 is not set
CONFIG_UBIFS_SILENCE_MSG=y
# CONFIG_FS_CRAMFS is not set
# CONFIG_YAFFS2 is not set
# CONFIG_FS_SQUASHFS is not set
#
# Library routines
#
# CONFIG_ADDR_MAP is not set
# CONFIG_BCH is not set
# CONFIG_CC_OPTIMIZE_LIBS_FOR_SPEED is not set
# CONFIG_DYNAMIC_CRC_TABLE is not set
CONFIG_HAVE_PRIVATE_LIBGCC=y
CONFIG_LIB_UUID=y
CONFIG_PRINTF=y
CONFIG_SPL_PRINTF=y
CONFIG_SPRINTF=y
CONFIG_SPL_SPRINTF=y
CONFIG_STRTO=y
CONFIG_SPL_STRTO=y
CONFIG_USE_PRIVATE_LIBGCC=y
CONFIG_SYS_HZ=1000
CONFIG_SPL_USE_TINY_PRINTF=y
# CONFIG_PANIC_HANG is not set
CONFIG_REGEX=y
CONFIG_LIB_RAND=y
# CONFIG_LIB_HW_RAND is not set
# CONFIG_SPL_TINY_MEMSET is not set
# CONFIG_TPL_TINY_MEMSET is not set
# CONFIG_BITREVERSE is not set
# CONFIG_TRACE is not set
# CONFIG_CMD_DHRYSTONE is not set
#
# Security support
#
# CONFIG_AES is not set
# CONFIG_RSA is not set
# CONFIG_ASYMMETRIC_KEY_TYPE is not set
# CONFIG_TPM is not set
# CONFIG_SPL_TPM is not set
#
# Android Verified Boot
#
#
# Hashing Support
#
CONFIG_SHA1=y
CONFIG_SHA256=y
# CONFIG_SHA512_ALGO is not set
# CONFIG_SHA_HW_ACCEL is not set
CONFIG_MD5=y
# CONFIG_SPL_MD5 is not set
#
# Compression Support
#
# CONFIG_LZ4 is not set
# CONFIG_LZMA is not set
# CONFIG_LZO is not set
CONFIG_GZIP=y
# CONFIG_ZLIB_UNCOMPRESS is not set
# CONFIG_BZIP2 is not set
CONFIG_ZLIB=y
# CONFIG_ZSTD is not set
# CONFIG_SPL_LZ4 is not set
# CONFIG_SPL_LZMA is not set
# CONFIG_SPL_LZO is not set
# CONFIG_SPL_GZIP is not set
# CONFIG_SPL_ZSTD is not set
# CONFIG_ERRNO_STR is not set
# CONFIG_HEXDUMP is not set
# CONFIG_GETOPT is not set
CONFIG_OF_LIBFDT=y
CONFIG_OF_LIBFDT_ASSUME_MASK=0
# CONFIG_OF_LIBFDT_OVERLAY is not set
CONFIG_SPL_OF_LIBFDT=y
CONFIG_SPL_OF_LIBFDT_ASSUME_MASK=0xff
# CONFIG_TPL_OF_LIBFDT is not set
CONFIG_TPL_OF_LIBFDT_ASSUME_MASK=0xff
#
# System tables
#
CONFIG_GENERATE_SMBIOS_TABLE=y
CONFIG_LIB_RATIONAL=y
CONFIG_SPL_LIB_RATIONAL=y
# CONFIG_SMBIOS_PARSER is not set
CONFIG_EFI_LOADER=y
CONFIG_EFI_VARIABLE_FILE_STORE=y
# CONFIG_EFI_VARIABLES_PRESEED is not set
CONFIG_EFI_VAR_BUF_SIZE=16384
CONFIG_EFI_DEVICE_PATH_TO_TEXT=y
CONFIG_EFI_LOADER_HII=y
CONFIG_EFI_UNICODE_COLLATION_PROTOCOL2=y
CONFIG_EFI_UNICODE_CAPITALIZATION=y
# CONFIG_EFI_UNICODE_COLLATION_PROTOCOL is not set
CONFIG_EFI_PLATFORM_LANG_CODES="en-US"
CONFIG_EFI_GRUB_ARM32_WORKAROUND=y
# CONFIG_EFI_LOAD_FILE2_INITRD is not set
# CONFIG_EFI_SECURE_BOOT is not set
# CONFIG_TEST_FDTDEC is not set
CONFIG_LIB_ELF=y
# CONFIG_PHANDLE_CHECK_SEQ is not set
# CONFIG_UNIT_TEST is not set
# CONFIG_SPL_UNIT_TEST is not set
#
# Tools options
#
CONFIG_MKIMAGE_DTC_PATH="dtc"
what is the problem?