We are basing a new HW design on the C6678 EVM kit. We are not planning to use the HyperLink SERDES function, but are planning to use one pair of the SGMII SERDES to/from an Ethernet PHY. We are tight on board space. For the SERDES supply, do we need to add all decoupling components (around 50) that are on the EVM kit reference design, keeping in mind we are using SGMII only?