Part Number: TDA4AP-Q1
Dear support,
I would like to builf the MCSPI examples with "ti-processor-sdk-rtos-j784s4-evm-09_00_00_02" but when calling the gmake command below I get the output "Nothing to be done for..."
C:\ti\ti_rtos_sdk\pdk_j784s4_09_00_00_45\packages\ti\build>gmake MCSPI_Baremetal_MasterSlave_TestApp BOARD=j784s4_evm CORE=mcu1_0
Nothing to be done for j784s4 MCSPI_Baremetal_MasterSlave_TestApp
In "pdk_j784s4_09_00_00_45/docs/userguide/j784s4/getting_started.html" the following is written: "If a library is not applicable for a given core or board, the make system will print message like below Nothing to be done for <BOARD> <CORE> <target>"
From the source file "main_mcspi_slave_mode.c" there is a define "defined(SOC_J784S4)", so it should be available for the used part.
Do you have any idea why I always get the output "Nothing to be done for..." and what do I need to do to generate the binary?
Best regards
Erwin