Other Parts Discussed in Thread: TDA4VH
Hi Team,
In the TDA4VH development board reference design, SERDES1 is used to connect to PCIe x4 lane CONN and SERDES0 is used to connect to PCIe x2 lane CONN as well as USBC.
1)
a. The reference clock SERDES1_REFCLK for SERDES1 is used to receive the clock signal. PCIe_REFCLK0_P/N_out is disconnected. (0ohm resistor in BOM is DNI)
b. The reference clock SERDES0_REFCLK for SERDES0 is disconnected (0ohm resistor in BOM is DNI). PCIE_REFCLK1_P/N_out is connected to the clock input.
Would you help share the intention of the above connections? Also, could you help share how to use a reference clock?
2) How to set the reference clock if the customer want to use SERDES0_TX2/RX2 from SERDES0 as SSTX/RX for USB A?
Could you help check this case? Thanks.
Best Regards,
Cherry