This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

building the sdk fails at cloning arago-project repository

Part Number: PROCESSOR-SDK-K2G


Hi,

I'm following along this video: https://www.ti.com/video/5768885091001 on building the SDK for my k2g-evm.

When running the following command:

./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-06.03.00.106-config.txt 

The part when it needs to clone meta-processor-sdk from arago-project.org hangs forever, since the domain was switched to some other place:

cloning repo meta-processor-sdk

Cloning into '/home/mgui/yocto/tisdk/sources/meta-processor-sdk'...
fatal: unable to access 'http://arago-project.org/git/projects/meta-processor-sdk.git/': Failed to connect to arago-project.org port 80: Connection refused
git failed... remaining attempts: 4    sleeping 15 seconds

The problem is that from https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-K2G 06.03.00.106 is the latest version for my evm.

I tried using a more recent configuration file, but then no recipes are provided for k2g-evm.

I'm using an ubuntu 18.04 host machine.

Is the k2g-evm still actively supported for building the SDK? I tried the demo SDK but for our needs we would need something closer to the yocto framework.

What is the most up-to-date way to build a linux image for this board?

Thanks