This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6655: Internal Temp Sensor?

Part Number: TMS320C6655

Does TI C6655 or C6657 have an internal temperature sensor ? 
OR
some register where it stores high temperature warning / fault ?

  • TK,

    The answer is "no". It does not have any internal temperature sensor.

    But an external temperature sensor shall be interfaced through SPI.

    Please refer datasheet of C6655 ---> page no: 47 

    5.7.9 SPI Peripheral

    The serial peripheral interconnect (SPI) module provides an interface between the DSP and other SPIcompliant devices. The primary intent of this interface is to allow for connection to an SPI ROM for boot. The SPI module on the C665x is supported only in master mode. Additional chip-level components can also be included, such as temperature sensors or an I/O expander.  

    Regards

    Shankari G