Part Number: PROCESSOR-SDK-AM335X
Hi All,
I am facing build issue while building the yocto project below is the log,
i am using 1.2. Building the SDK — Processor SDK Linux for AM335X Documentation steps.
host system = ubuntu18.04
ERROR: core-image-minimal-1.0-r0 do_rootfs: The postinstall intercept hook 'update_pixbuf_cache' failed, details in /home/source/build/arago-tmp-external-arm-glibc/work/am335x_evm-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs
with exit code '1'
NOTE: Tasks Summary: Attempted 3557 tasks of which 1934 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 3 seconds
Can anyone please help ASAP .in this as i am not able to proceed further.
Andreas Dannenberg can you please help me out here.. what i need to update.