Hello Champs,
Customer is using PCIe wifi with Intel9260 on TDA4 AI board, but the bandwidth is only 20MHz, the hostapd only supports cfg80211g. How to improve the bandwidth to 40/80MHz cfg80211n?
root@tda4vm-sk:/usr/share/intel9260# iw wlp1s0 info
Interface wlp1s0
ifindex 7
wdev 0x1
addr 00:e1:8c:c9:7f:34
ssid J7SK-AP_8cc97f
type AP
wiphy 0
channel 11 (2462 MHz), width: 20 MHz, center1: 2462 MHz
txpower 22.00 dBm
multicast TXQ:
qsz-byt qsz-pkt flows drops marks overlmt hashcol tx-bytes tx-packets
0 0 34 0 0 0 0 8974 34
Thanks
Regards
Shine