The following is my operations:
1.setup ezsdk_5_01_01_80
2.rebuild the SD card with ${EZSDK}/bin/mksdboot.sh --device /dev/sdb --sdk ${EZSDK}
3.check the switch sw3 sw4
4.power on
But the serial only print here“ “Uncompressing Linux......... done, booting the kerne ”,
I reboot the demo board with power ,and md the address of __log_buf,and debug ,find that, the content in the buffer as follow:
................
................
....l.i2c2_scl..
................
................
................
....sda.i2c2_sda
................
................
................
....vpss device
.<3>pm_dbg_init:
only OMAP3 supp
orted.<6>Registe
red ti81xx_fb de
vice............
................
................
....pcie: Settin
g up Host Contro
ller............
................
....e mapped @0x
d0820000........
................
................
and the kernel stop at the function start_kernel(void) –>rest_init()->schedule()
and I did no change to the kernel and u-boot,
and my demo board version is : main board version :E and daughter board version is :C
how can I boot the demo baord with my SD card;