Other Parts Discussed in Thread: TPS65023, AM3517
Hi,
I am testing on custom board similar with am3517evm except LCD, I substitute a 7" LCD for 4"3' LCD. (7" LCD: 800*480, CLK=33300; 4"3' LCD: 480*272,CLK=9000)
I am booting from NAND, and xloader, uboot, uImage, ubi.img are all on NAND, no MMC is attached.
Each time when I first power on the board, "omaplfb: OMAPLFB_Init: OMAPLFBInit failed" will show on the console, and android system can't start up.
but if I reboot (just push the reboot button, not power off then power on), then the android system can start up successfully.
however, if I power off, then power on, the same case will appear, "omaplfb: OMAPLFB_Init: OMAPLFBInit failed" will come up on the console.
If boot from MMC, no such problem.
So, why do I have to try boot second time after first fail for the error "omaplfb: OMAPLFB_Init: OMAPLFBInit failed"?
what is the difference between second reboot and first power on?
The console log is attached. 3884.OMAPLFBInit failed.txt
Thanks,
Kevin