Hello Champs,
During emmc booting, we an use ls mmc 0:1 command to check rootfs partition and files. How to check the boot0 and boot1 partitions?
Thanks
Regards
Shine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
During emmc booting, we an use ls mmc 0:1 command to check rootfs partition and files. How to check the boot0 and boot1 partitions?
The SDK User's Guide has some explanation on this, see https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_00_00_03/exports/docs/linux/Foundational_Components/U-Boot/UG-Memory.html#booting-tiboot3-bin-tispl-bin-and-u-boot-img-from-emmc-boot-partition-for-k3-class-of-socs
Basically, you can switch to the boot0 partition using the `mmc dev 0 1` command, and then you can access the data (in raw format, because there's no filesystem!) using the usual `mmc read` and `mmc write commands. Similarly, for accessing the boot1 partition, first switch to that partition using `mmc dev 0 2`, before doing any raw access.
Regards, Andreas
Hi Andreas,
Thank you very much.
Customer asked which partition for mmc dev 0 0 command.
Thanks
Regards
Shine
Hi Shine,
The last zero in the `mmc dev 0 0` command used as the parameter for the partition refers to the user data partition/area (also known as UDA). If you don't specify this last partition parameter it actually defaults to `0` so usually it is not specified at all in this case.
Regards, Andreas