Hi guys!!
I have configured the environment in order to build the sources DSPLINK for GPP and DSP-side. There are errors when I try to do "make" in a prompt of Linux. I show the answer below:
Building kernel side code using kbuild
make PROFILE=DEBUG -C /home/user/omap3530/AM35x-OMAP35x-PSP-SDK-03.00.00.05/src/kernel/linux-03.00.00.05 SUBDIRS=/home/user/dsplink/gpp/src ARCH=arm CROSS_COMPILE=/home/user/toolchains/git/arm-2009q1-203/bin/arm-none-linux-gnueabi- modules
make: *** /home/user/omap3530/AM35x-OMAP35x-PSP-SDK-03.00.00.05/src/kernel/linux-03.00.00.05: No existe el fichero o el directorio. Alto.
make: *** [debug] Error 2
The paths have been changed and revised but there are some changes that not applied...I have doutbs about that where is the problem...Any suggestion??
Thanks in advance. Regards.
Óscar