This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg: DSS mode configuration to mode 0

Iam looking to change the DSS mode to 0,currently in EVM and in beagle MODE 3/7 is configured from the software and it is working fine.

We are trying to interface a custom LCD (24-bit) and the resolution is 320x240. We are using PCLK frequency less than 60Mhz and we  have provided option in our hardware to support only mode 0 (DSS_DATA[0:23]). We are  unable to configure to mode 0, we can tell this because we are able to see the data in all the rest of the lines except DSS_DATA[0:5].

Kindly  suggest us the solution to configure to mode 0 which would enable to us to see the data on DSS_DATA[0:5] .

 

thanks