We are booting the board with SD card . SD card are divided into two parts boot and rootfs and loaded zimage,MLO,U-boot .
When we are booting from SD-card board is booting after continues on and off board is not booting from Sd card.
We observed that SD Protect is high and SD Detect Pin is low even though while booting from Sd Card
We are using 4GB SD-card and we also tried with another 16 GB SD card then also we observed same Problem
i am attaching Schematics of SD card below:
Now , U44 IC present in above Schematics is removed and 2 & 4 pins and 1 & 3 pins are shorted for SD Detect pins to be low .
We didn't understand why board is not booting from SD card Sometimes.
Regards,
Mounika