This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: enable keyboard and mouse

Part Number: TDA4VH-Q1

Hello all,

I have this board: https://www.ti.com/tool/J784S4XEVM

There are 2 USBs type A, which the user guide specifies:

"The EVM supports two USB2.0 Type A interfaces [J5] via an on-board USB hub. These ports can only function as Host. The VBUS output for each port is limited to 0.5 A. The processor supports a single USB interface. Therefore, the user must configure for either the USB2.0 Type A interface or the USB3.1 Type C interface. Both cannot be operated simultaneously."

How to enable those 2 USB to be used for mouse and keyboard?

Br, Mircea