Hi,
Anybody know what format is the camera input?
I think that the camera input format is YCbCr 4:2:2 - ITU-R BT.656.
I would like some informations about the camera input as applications note or datasheets.
Thanks!
Juliano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Anybody know what format is the camera input?
I think that the camera input format is YCbCr 4:2:2 - ITU-R BT.656.
I would like some informations about the camera input as applications note or datasheets.
Thanks!
Juliano
Ok. I found on datasheet and others applications note that beagleboard connector to camera is YCbCr 4:2:2 10-bits, but I have other question.
Somebody know what is best level converter that I can used between the beagleboard and an camera with 5 V of I/O.
Thanks!
Juliano.
It is very important you read the sprugn4q.pdf. Specially the chapter 6. ISP interface on DM3730 works with several kinds of video interface.
The input on ISP interface work with 1.8V. So, to interface your camera you need a level translator.
Which is the camera that you trying connect?