Part Number: AM623
Hello,
I have a device with two processors. One is an AM6234, and the other is a processor from another manufacturer. I am attempting to connect the two processors via an RGMII fixed-link connection with no PHY in between. I am trying to find the best way to add the necessary setup time on the RGMII clock lines, and am limited on board space so adding a PHY is not an option. Does the AM6234 support adding internal delay in the Ethernet MAC?