Other Parts Discussed in Thread: TDA4VL, TDA4VM
Hello,
USB SSD is connected to type c port on TDA4VL EVM but it works in USB 2.0.
output of "lsusb -t" on TDA4VL
/: Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M /: Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M |__ Port 1: Dev 2, If 0, Class=Mass Storage, Driver=usb-storage, 480M
But USB3.0 on TDA4VM, with same SSD and same type c cable
/: Bus 04.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M /: Bus 03.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M |__ Port 1: Dev 2, If 0, Class=Hub, Driver=hub/4p, 480M |__ Port 2: Dev 3, If 0, Class=Human Interface Device, Driver=usbhid, 1.5M /: Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M |__ Port 1: Dev 2, If 0, Class=Mass Storage, Driver=usb-storage, 5000M /: Bus 01.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 480M
How can I enable USB 3.0 on TDA4VL EVM?
if lsusb output has "/: Bus 02.Port 1: Dev 1, Class=root_hub, Driver=xhci-hcd/1p, 5000M", is enabled SERDES for USB 3.0 ?
Best regards,
Wilson