This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BEAGL-BONE-BLACK: Yes

Part Number: BEAGL-BONE-BLACK

Hi Expert ,

I am trying to setup wi-link8 with beagle bone black . As part of the compilation process of wi-link module with R8.8 version,  I am trying to clone some of the required module from git.

using "./build_wl18xx.sh init". I am facing following issue while accessing or cloning from git like "git clone git://github.com/tgraf/libnl.git" .

I have gone through the internet to resolve the issue so and changed the URL to github.com/.../libnl.git then i was able to clone it . but when i am trying to do the same with "./build_wl18xx.sh init" script then now facing new issue like 

Document used for the steps : www.ti.com/.../swru561a.pdf

below is the logs if running "./build_wl18xx.sh init" with change URL git://github.com/tgraf/libnl.git

Cloning into: libnl
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/libnl'...
fatal: unable to connect to github.com:
github.com[0: 20.205.243.166]: errno=Connection timed out

below is the logs if running"./build_wl18xx.sh init" with change URL github.com/.../libnl.git

Cloning into: libnl
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/libnl'...
fatal: unable to access 'github.com/.../': error setting certificate verify locations:
CAfile: /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sy

below is the logs if running"./build_wl18xx.sh init" with change URL git://github.com/

Using user defined kernel
Makefile was found. Kernel version was set to 20.4.19.
***** initializing workspace (w/o build) *****
Cloning into: kernel
Cloning into: openssl
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/openssl'...
fatal: unable to connect to github.com:
github.com[0: 20.205.243.166]: errno=Connection timed out

Cloning into: libnl
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/libnl'...
fatal: unable to connect to github.com:
github.com[0: 20.205.243.166]: errno=Connection timed out

Cloning into: crda
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/crda'...
fatal: read error: Connection reset by peer
Cloning into: wireless_regdb
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/wireless_regdb'...
fatal: read error: Connection reset by peer
Cloning into: driver
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/driver'...
fatal: read error: Connection reset by peer
Cloning into: hostap
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/hostap'...
fatal: read error: Connection reset by peer
Cloning into: ti_utils
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/ti_utils'...
fatal: read error: Connection reset by peer
Cloning into: fw_download
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/fw_download'...
fatal: read error: Connection reset by peer
Cloning into: scripts_download
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/scripts_download'...
fatal: read error: Connection reset by peer
Cloning into: backports
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/backports'...
fatal: read error: Connection reset by peer
Cloning into: iw
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/iw'...
fatal: read error: Connection reset by peer
Cloning into: uim
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/uim'...
fatal: read error: Connection reset by peer
Cloning into: bt-firmware
Cloning into '/home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/bt-firmware'...
fatal: read error: Connection reset by peer
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/openssl: No such file or directory

Checking out branch OpenSSL_1_0_2d in repo openssl
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/libnl: No such file or directory

Checking out branch libnl3_2_25 in repo libnl
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/crda: No such file or directory

Checking out branch master in repo crda
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/wireless_regdb: No such file or directory

Checking out branch master-2017-03-07 in repo wireless_regdb
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/driver: No such file or directory

Checking out branch upstream_44 in repo driver
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/hostap: No such file or directory

Checking out branch upstream_25_rebase in repo hostap
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/ti_utils: No such file or directory

Checking out branch master in repo ti_utils
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/fw_download: No such file or directory

Checking out branch master in repo fw_download
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/scripts_download: No such file or directory

Checking out branch sitara-scripts in repo scripts_download
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/backports: No such file or directory

Checking out branch upstream_44 in repo backports
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/iw: No such file or directory

Checking out branch v4.1 in repo iw
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
fatal: not a git repository (or any of the parent directories): .git
./build_wl18xx.sh: line 110: cd: /home/zakir/ti-processor-sdk-linux-am335x-evm-06.00.00.07/wl8-build/build-utilites-master/src/uim: No such file or directory

kindly help me to resolve the issue .

Regards 

Jakir Hussain

7838857428/7982214697


 

  • Hi Jakir,

    It seems you are having trouble cloning the repo. Perhaps you are behind a firewall? Do you have any issue cloning the repos manually?

  • Jakir,

    This is not a beagle-bone-black or processor question. For future reference please post it in the right forum.

    As sabeeh said, its mostly your local build machine proxy settings .

    --

    The instructions from https://www.ti.com/lit/ug/swru561a/swru561a.pdf worked fine, just tried it. ( closing this ticket)

    ~/test/build-utilites$ ./build_wl18xx.sh init
    ***** *** Entering to create the setup environment based on setup-env file ..... *****
    Using user defined kernel
    Makefile was found. Kernel version was set to 6.1.59.
    ***** initializing workspace (w/o build) *****
    Cloning into: openssl
    Cloning into '/home/praneeth/test/build-utilites/src/openssl'...
    remote: Enumerating objects: 464065, done.
    remote: Counting objects: 100% (39576/39576), done.
    remote: Compressing objects: 100% (1581/1581), done.
    remote: Total 464065 (delta 38416), reused 38032 (delta 37995), pack-reused 424489
    Receiving objects: 100% (464065/464065), 214.72 MiB | 7.40 MiB/s, done.
    Resolving deltas: 100% (336092/336092), done.
    Cloning into: libnl
    Cloning into '/home/praneeth/test/build-utilites/src/libnl'...
    remote: Enumerating objects: 16493, done.
    remote: Counting objects: 100% (4245/4245), done.
    remote: Compressing objects: 100% (864/864), done.
    remote: Total 16493 (delta 3486), reused 3986 (delta 3345), pack-reused 12248
    Receiving objects: 100% (16493/16493), 5.95 MiB | 9.03 MiB/s, done.
    Resolving deltas: 100% (11862/11862), done.
    Cloning into: wireless_regdb
    Cloning into '/home/praneeth/test/build-utilites/src/wireless_regdb'...
    remote: Enumerating objects: 1641, done.
    remote: Counting objects: 100% (19/19), done.
    remote: Compressing objects: 100% (18/18), done.
    remote: Total 1641 (delta 7), reused 0 (delta 0), pack-reused 1622
    Receiving objects: 100% (1641/1641), 448.44 KiB | 6.06 MiB/s, done.
    Resolving deltas: 100% (1155/1155), done.
    Cloning into: hostap
    Cloning into '/home/praneeth/test/build-utilites/src/hostap'...
    remote: Counting objects: 83795, done.
    remote: Compressing objects: 100% (18961/18961), done.
    remote: Total 83795 (delta 65781), reused 82449 (delta 64577)
    Receiving objects: 100% (83795/83795), 33.20 MiB | 10.47 MiB/s, done.
    Resolving deltas: 100% (65781/65781), done.
    Cloning into: ti_utils
    Cloning into '/home/praneeth/test/build-utilites/src/ti_utils'...
    remote: Counting objects: 2597, done.
    remote: Compressing objects: 100% (912/912), done.
    remote: Total 2597 (delta 1838), reused 2312 (delta 1662)
    Receiving objects: 100% (2597/2597), 17.85 MiB | 19.08 MiB/s, done.
    Resolving deltas: 100% (1838/1838), done.
    Cloning into: fw_download
    Cloning into '/home/praneeth/test/build-utilites/src/fw_download'...
    remote: Counting objects: 562, done.
    remote: Compressing objects: 100% (256/256), done.
    remote: Total 562 (delta 328), reused 524 (delta 303)
    Receiving objects: 100% (562/562), 12.40 MiB | 15.97 MiB/s, done.
    Resolving deltas: 100% (328/328), done.
    Cloning into: scripts_download
    Cloning into '/home/praneeth/test/build-utilites/src/scripts_download'...
    remote: Counting objects: 1613, done.
    remote: Compressing objects: 100% (847/847), done.
    remote: Total 1613 (delta 939), reused 1258 (delta 745)
    Receiving objects: 100% (1613/1613), 246.51 KiB | 2.62 MiB/s, done.
    Resolving deltas: 100% (939/939), done.
    Cloning into: iw
    Cloning into '/home/praneeth/test/build-utilites/src/iw'...
    remote: Enumerating objects: 3470, done.
    remote: Total 3470 (delta 0), reused 0 (delta 0), pack-reused 3470
    Receiving objects: 100% (3470/3470), 796.57 KiB | 14.75 MiB/s, done.
    Resolving deltas: 100% (2357/2357), done.

    Checking out branch OpenSSL_1_1_1b in repo openssl
    Checking out files: 100% (20375/20375), done.
    Note: checking out 'OpenSSL_1_1_1b'.

    You are in 'detached HEAD' state. You can look around, make experimental
    changes and commit them, and you can discard any commits you make in this
    state without impacting any branches by performing another checkout.

    If you want to create a new branch to retain commits you create, you may
    do so (now or later) by using -b with the checkout command again. Example:

    git checkout -b <new-branch-name>

    HEAD is now at 50eaac9f33 Prepare for 1.1.1b release

    Checking out branch libnl3_4_0 in repo libnl
    Note: checking out 'libnl3_4_0'.

    You are in 'detached HEAD' state. You can look around, make experimental
    changes and commit them, and you can discard any commits you make in this
    state without impacting any branches by performing another checkout.

    If you want to create a new branch to retain commits you create, you may
    do so (now or later) by using -b with the checkout command again. Example:

    git checkout -b <new-branch-name>

    HEAD is now at 3fe3454b libnl-3.4.0 release

    Checking out branch master-2020-04-29 in repo wireless_regdb
    Note: checking out 'master-2020-04-29'.

    You are in 'detached HEAD' state. You can look around, make experimental
    changes and commit them, and you can discard any commits you make in this
    state without impacting any branches by performing another checkout.

    If you want to create a new branch to retain commits you create, you may
    do so (now or later) by using -b with the checkout command again. Example:

    git checkout -b <new-branch-name>

    HEAD is now at 222442d wireless-regdb: update regulatory database based on preceding changes

    Checking out branch upstream_29_rebase in repo hostap
    Branch 'upstream_29_rebase' set up to track remote branch 'upstream_29_rebase' from 'origin'.
    Switched to a new branch 'upstream_29_rebase'

    Checking out branch master in repo ti_utils
    Already on 'master'
    Your branch is up to date with 'origin/master'.

    Checking out branch master in repo fw_download
    Already on 'master'
    Your branch is up to date with 'origin/master'.

    Checking out branch sitara-scripts in repo scripts_download
    Branch 'sitara-scripts' set up to track remote branch 'sitara-scripts' from 'origin'.
    Switched to a new branch 'sitara-scripts'

    Checking out branch v4.14 in repo iw
    Note: checking out 'v4.14'.

    You are in 'detached HEAD' state. You can look around, make experimental
    changes and commit them, and you can discard any commits you make in this
    state without impacting any branches by performing another checkout.

    If you want to create a new branch to retain commits you create, you may
    do so (now or later) by using -b with the checkout command again. Example:

    git checkout -b <new-branch-name>

    HEAD is now at f328848 bump version to 4.14
    python-m2crypto is missing
    Please use 'sudo apt-get install python-m2crypto'
    Do you want to install it now [y/n] ? (requires sudo) n
    python-m2crypto was not installed. leaving build.