Part Number: DRA829J-Q1
Other Parts Discussed in Thread: DRA829
Dears,
What we tested was the impedance between VDA_DLL_0V8 and DGND. When the first batch of PCBAs were produced (total: 36 PCS PCBA), 95% of the PCBAs had an impedance value between VDA_DLL_0V8 and DGND of 11k-12K (Expected Value: 5K-20k) , when producing the second batch of PCBA (total: 70 PCS PCBA), we found that nearly 50% of the PCBA, the impedance value between AVDA_DLL_0V8 and DGND was around 400Ω.
This VDA_DLL_0V8 is generated by TPS65941213RWERQ1, and then directly provides the working voltage to N9_ VDDA_0P8_PLL_DDR and Y9_ VDDA_0P8_DLL_MMC0 of MCU_ DRA829.
Should I appropriately relax the Expected Value based on the production situation? Are there any big risks?

Thanks