Hi
We have setup AM5728 processor (PHYTEC SoM) to communicate with Xilinx Zynq FPGA through PCIe Endpoint (PCIe Lane 2).
It was working in older BSP build (18.x), After we updated to latest BSP (20.1.2), The Endpoint is not being detected on FPGA side.
And also dmesg showed this error message:
[ 0.572031] dra7-pcie 51800000.pcie_ep: Linked as a consumer to phy-4a095000.pciephy.2 [ 0.572207] dra7-pcie 51800000.pcie_ep: GPIO lookup for consumer pcie-clk-oe [ 0.572215] dra7-pcie 51800000.pcie_ep: using device tree for GPIO lookup [ 0.572235] of_get_named_gpiod_flags: can't parse 'pcie-clk-oe-gpios' property of node '/ocp/axi@1/pcie_ep@51800000[0]' [ 0.572251] of_get_named_gpiod_flags: can't parse 'pcie-clk-oe-gpio' property of node '/ocp/axi@1/pcie_ep@51800000[0]' [ 0.572260] dra7-pcie 51800000.pcie_ep: using lookup tables for GPIO lookup [ 0.572269] dra7-pcie 51800000.pcie_ep: No GPIO consumer pcie-clk-oe found [ 0.572278] dra7-pcie 51800000.pcie_ep: GPIO lookup for consumer pcie-reset [ 0.572285] dra7-pcie 51800000.pcie_ep: using device tree for GPIO lookup [ 0.572301] of_get_named_gpiod_flags: can't parse 'pcie-reset-gpios' property of node '/ocp/axi@1/pcie_ep@51800000[0]' [ 0.572316] of_get_named_gpiod_flags: can't parse 'pcie-reset-gpio' property of node '/ocp/axi@1/pcie_ep@51800000[0]' [ 0.572323] dra7-pcie 51800000.pcie_ep: using lookup tables for GPIO lookup [ 0.572331] dra7-pcie 51800000.pcie_ep: No GPIO consumer pcie-reset found [ 0.572469] dra7-pcie 51800000.pcie_ep: Dropping the link to phy-4a095000.pciephy.2 [ 0.572511] dra7-pcie: probe of 51800000.pcie_ep failed with error -22
Any suggestions ?
Thanks & Regards,
Sujan