This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: Linux bootup time optimization

Part Number: SK-AM62

Hello,

I need some help to optimize the linux bootup time for SK-AM62 EVM.

I followed the instructions on '1.2 Building the SDK' from 'Processor SDK Linux for AM62x' and compiled the linux and the rootfs with the command `MACHINE=am62xx-evm bitbake -k tisdk-base-image`.

With a bootable SD card, it takes about 10 seconds to boot without modifying any default configuration. Uboot and the linux kernel together takes about 2.5 seconds but once "Welcome to Arago 2023.04!" is shown, it takes extra 7-8 seconds until it is fully booted. The full bootup log is attached in this post.

I tried to disable the unnecessary services and drivers through `MACHINE=am62xx-evm bitbake -c menuconfig virtual/kernel` (e.g. network, wlan, nfs) but it didn't make any significant difference (~1 second recution).

I would like to know:
(1) What would be the possible ways to optimize the bootup time for Arago project?
(2) Is there any official patch/support for Buildroot so that I can use it instead of Yocto project?
(3) I would like to test Bootgraph, but failed to add 'printk.time=y initcall_debug debug' on the kernel command line parameter. Could you guide me how to add the optional kernel command line parameter?

Thank you in advance.

�
U-Boot SPL 2023.04 (Oct 17 2023 - 08:42:39 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Trying to boot from MMC2
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.7(release):v2.7.0-359-g1309c6c80
NOTICE:  BL31: Built : 08:36:10, Oct 17 2023
I/TC: 
I/TC: OP-TEE version: 3.19.0-15-gd6c5d0037 (gcc version 11.3.1 20220712 (Arm GNU Toolchain 11.3.Rel1)) #1 Mon Oct 16 23:34:46 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2023.04 (Oct 17 2023 - 08:44:25 +0900)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 1856 bytes
Error (-2): cannot determine file size
Trying to boot from MMC2


U-Boot 2023.04 (Oct 17 2023 - 08:44:25 +0900)

SoC:   AM62X SR1.0 GP
Model: Texas Instruments AM625 SK
EEPROM not available at 80, trying to read at 81
Board: AM62-SKEVM rev E3
DRAM:  2 GiB
Core:  72 devices, 32 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial
Out:   serial
Err:   serial
Net:   eth0: ethernet@8000000port@1
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
Failed to load 'uEnv.txt'
## Error: "main_cpsw0_qsgmii_phyinit" not defined
20593152 bytes read in 231 ms (85 MiB/s)
57500 bytes read in 16 ms (3.4 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=ff700000 size=8ca000 flags=4)
   Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
Working FDT set to 8feee000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.1.33-g40c32565ca (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Thu Jul  6 14:17:24 UTC 2023
[    0.000000] Machine model: Texas Instruments AM625 SK
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009c7fffff]
[    0.000000]   node   0: [mem 0x000000009c800000-0x000000009e6fffff]
[    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
[    0.000000]   node   0: [mem 0x000000009e780000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ff6fffff]
[    0.000000]   node   0: [mem 0x00000000ff700000-0x00000000fffc9fff]
[    0.000000]   node   0: [mem 0x00000000fffca000-0x00000000ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),98048k@32m(ospi.rootfs),256k@130816k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=aa6e955e-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 1838092K/2097152K available (12480K kernel code, 1294K rwdata, 4040K rodata, 2176K init, 498K bss, 127988K reserved, 131072K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] 	Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008542] Console: colour dummy device 80x25
[    0.013136] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023819] pid_max: default: 32768 minimum: 301
[    0.028595] LSM: Security Framework initializing
[    0.033449] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.041034] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.050862] cblist_init_generic: Setting adjustable number of callback queues.
[    0.058323] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.064623] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.071026] rcu: Hierarchical SRCU implementation.
[    0.075933] rcu: 	Max phase no-delay instances is 1000.
[    0.081543] Platform MSI: msi-controller@1820000 domain created
[    0.087862] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.097703] EFI services will not be available.
[    0.102639] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
I/TC: Secondary CPU 2 initializing
I/TC: Secondary CPU 2 switching to normal world boot
I/TC: Secondary CPU 3 initializing
I/TC: Secondary CPU 3 switching to normal world boot
[    0.115962] Detected VIPT I-cache on CPU1
[    0.116081] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.116100] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
[    0.116158] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.124886] Detected VIPT I-cache on CPU2
[    0.124975] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[    0.124990] GICv3: CPU2: using allocated LPI pending table @0x0000000080070000
[    0.125024] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.133692] Detected VIPT I-cache on CPU3
[    0.133782] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[    0.133796] GICv3: CPU3: using allocated LPI pending table @0x0000000080080000
[    0.133829] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.133900] smp: Brought up 1 node, 4 CPUs
[    0.213612] SMP: Total of 4 processors activated.
[    0.218425] CPU features: detected: 32-bit EL0 Support
[    0.223691] CPU features: detected: CRC32 instructions
[    0.229010] CPU: All CPU(s) started at EL2
[    0.233207] alternatives: applying system-wide alternatives
[    0.240798] devtmpfs: initialized
[    0.252364] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.262366] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.273938] pinctrl core: initialized pinctrl subsystem
[    0.279924] DMI not present or invalid.
[    0.284500] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.291767] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.299335] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.307448] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.315636] audit: initializing netlink subsys (disabled)
[    0.321347] audit: type=2000 audit(0.216:1): state=initialized audit_enabled=0 res=1
[    0.321835] thermal_sys: Registered thermal governor 'step_wise'
[    0.329281] thermal_sys: Registered thermal governor 'power_allocator'
[    0.335470] cpuidle: using governor menu
[    0.346345] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.353377] ASID allocator initialised with 65536 entries
[    0.369758] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[    0.380983] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
[    0.391912] KASLR disabled due to lack of seed
[    0.403645] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.410619] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.417029] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.423969] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.430377] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.437317] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.443725] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.450664] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.458878] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[    0.468995] iommu: Default domain type: Translated 
[    0.474058] iommu: DMA domain TLB invalidation policy: strict mode 
[    0.480762] SCSI subsystem initialized
[    0.484976] usbcore: registered new interface driver usbfs
[    0.490634] usbcore: registered new interface driver hub
[    0.496126] usbcore: registered new device driver usb
[    0.501854] pps_core: LinuxPPS API ver. 1 registered
[    0.506938] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.516289] PTP clock support registered
[    0.520421] EDAC MC: Ver: 3.0.0
[    0.524580] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[    0.531723] FPGA manager framework
[    0.535304] Advanced Linux Sound Architecture Driver Initialized.
[    0.542563] clocksource: Switched to clocksource arch_sys_counter
[    0.549067] VFS: Disk quotas dquot_6.6.0
[    0.553121] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.566133] NET: Registered PF_INET protocol family
[    0.571446] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.580703] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.589515] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.597455] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.605659] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.613657] TCP: Hash tables configured (established 16384 bind 16384)
[    0.620576] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.627505] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.635053] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.641327] RPC: Registered named UNIX socket transport module.
[    0.647407] RPC: Registered udp transport module.
[    0.652218] RPC: Registered tcp transport module.
[    0.657027] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.663618] NET: Registered PF_XDP protocol family
[    0.668532] PCI: CLS 0 bytes, default 64
[    0.673357] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.683453] Initialise system trusted keyrings
[    0.688281] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    0.700734] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.707432] NFS: Registering the id_resolver key type
[    0.712660] Key type id_resolver registered
[    0.716938] Key type id_legacy registered
[    0.721102] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.727958] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.735724] 9p: Installing v9fs 9p2000 file system support
[    0.775897] Key type asymmetric registered
[    0.780090] Asymmetric key parser 'x509' registered
[    0.785128] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[    0.792864] io scheduler mq-deadline registered
[    0.797504] io scheduler kyber registered
[    0.804921] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[    0.811484] pinctrl-single f4000.pinctrl: 171 pins, size 684
[    0.818270] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[    0.831931] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.846778] loop: module loaded
[    0.851340] megasas: 07.719.03.00-rc1
[    0.859231] tun: Universal TUN/TAP device driver, 1.6
[    0.865162] thunder_xcv, ver 1.0
[    0.868516] thunder_bgx, ver 1.0
[    0.871844] nicpf, ver 1.0
[    0.875019] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[    0.882408] hns3: Copyright (c) 2017 Huawei Corporation.
[    0.887900] hclge is initializing
[    0.891309] e1000: Intel(R) PRO/1000 Network Driver
[    0.896300] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.902211] e1000e: Intel(R) PRO/1000 Network Driver
[    0.907285] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.913367] igb: Intel(R) Gigabit Ethernet Network Driver
[    0.918886] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.924607] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.931014] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.937197] sky2: driver version 1.30
[    0.941656] VFIO - User Level meta-driver version: 0.3
[    0.947753] usbcore: registered new interface driver usb-storage
[    0.954706] i2c_dev: i2c /dev entries driver
[    0.961282] sdhci: Secure Digital Host Controller Interface driver
[    0.967646] sdhci: Copyright(c) Pierre Ossman
[    0.972606] Synopsys Designware Multimedia Card Interface Driver
[    0.979208] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.986049] ledtrig-cpu: registered to indicate activity on CPUs
[    0.992414] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.999380] usbcore: registered new interface driver usbhid
[    1.005085] usbhid: USB HID core driver
[    1.010338] optee: probing for conduit method.
[    1.014943] optee: revision 3.19 (d6c5d003)
[    1.015272] optee: dynamic shared memory is enabled
[    1.025066] optee: initialized driver
[    1.030880] Initializing XFRM netlink socket
[    1.035303] NET: Registered PF_PACKET protocol family
[    1.040623] 9pnet: Installing 9P2000 support
[    1.045056] Key type dns_resolver registered
[    1.049860] registered taskstats version 1
[    1.054086] Loading compiled-in X.509 certificates
[    1.067852] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
[    1.131303] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    1.138887] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[    1.145923] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
[    1.151904] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[    1.160253] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    1.169491] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    1.179503] ti-udma 485c0100.dma-controller: Number of rings: 82
[    1.187726] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[    1.198898] ti-udma 485c0000.dma-controller: Number of rings: 150
[    1.208981] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[    1.219179] printk: console [ttyS2] disabled
[    1.223637] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 239, base_baud = 3000000) is a 8250
[    1.232537] printk: console [ttyS2] enabled
[    1.232537] printk: console [ttyS2] enabled
[    1.240997] printk: bootconsole [ns16550a0] disabled
[    1.240997] printk: bootconsole [ns16550a0] disabled
[    1.254061] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[    1.259182] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
[    1.266143] Creating 7 MTD partitions on "fc40000.spi.0":
[    1.271538] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    1.278283] 0x000000080000-0x000000280000 : "ospi.tispl"
[    1.284715] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    1.291214] 0x000000680000-0x0000006c0000 : "ospi.env"
[    1.297407] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[    1.304227] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    1.310855] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    1.319198] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.362596] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.372477] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[    1.380588] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
[    1.388712] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[    1.401567] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[    1.408696] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.415202] pps pps0: new PPS source ptp0
[    1.419498] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    1.430015] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[    1.441452] mmc0: CQHCI version 5.10
[    1.447939] pca953x 1-0022: supply vcc not found, using dummy regulator
[    1.454681] pca953x 1-0022: using AI
[    1.481262] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    1.488075] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[    1.496920] mmc1: CQHCI version 5.10
[    1.496968] mmc2: CQHCI version 5.10
[    1.510031] ALSA device list:
[    1.513029]   No soundcards found.
[    1.536461] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[    1.543638] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    1.551734] Waiting for root device PARTUUID=aa6e955e-02...
[    1.581869] mmc0: Command Queue Engine enabled
[    1.586346] mmc0: new HS200 MMC card at address 0001
[    1.592150] mmcblk0: mmc0:0001 S0J56X 14.8 GiB 
[    1.600732]  mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14
[    1.603927] mmc1: new ultra high speed SDR104 SDXC card at address aaaa
[    1.608921] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB 
[    1.614477] mmcblk1: mmc1:aaaa SN64G 59.5 GiB 
[    1.619892] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB 
[    1.625300]  mmcblk1: p1 p2
[    1.629195] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (240:0)
[    2.204009] EXT4-fs (mmcblk1p2): recovery complete
[    2.210704] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[    2.219339] VFS: Mounted root (ext4 filesystem) on device 179:66.
[    2.225669] devtmpfs: mounted
[    2.230139] Freeing unused kernel memory: 2176K
[    2.234776] Run /sbin/init as init process
[    2.369818] systemd[1]: System time before build time, advancing clock.
[    2.421513] NET: Registered PF_INET6 protocol family
[    2.428416] Segment Routing with IPv6
[    2.432188] In-situ OAM (IOAM) with IPv6
[    2.461656] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    2.493567] systemd[1]: Detected architecture arm64.

Welcome to Arago 2023.04!

[    2.576041] systemd[1]: Hostname set to <am62xx-evm>.
[    2.583935] systemd[1]: Initializing machine ID from random generator.
[    2.697550] systemd-sysv-generator[159]: SysV service '/etc/init.d/resize_rootfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.722864] systemd-sysv-generator[159]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.749114] systemd-sysv-generator[159]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.773583] systemd-sysv-generator[159]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.798386] systemd-sysv-generator[159]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.822203] systemd-sysv-generator[159]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.846016] systemd-sysv-generator[159]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    2.872378] systemd-sysv-generator[159]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    3.188910] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    3.261899] systemd[1]: Queued start job for default target Multi-User System.
[    3.327923] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    3.353650] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    3.377564] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    3.401115] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    3.423188] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    3.447085] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[    3.471202] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    3.486864] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    3.506931] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    3.523014] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    3.589323] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    3.611131] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    3.651799] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    3.675656] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    3.700698] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    3.724734] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    3.749553] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    3.768842] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    3.794111] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    3.817058] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    3.841284] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    3.903273] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    3.930666] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    3.966758] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    3.984022] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[    4.027441] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    4.053031] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    4.083170] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    4.115014] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    4.146074] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    4.160608] fuse: init (API version 7.37)
[    4.174727] systemd[1]: Starting Start psplash boot splash screen...
         Starting Start psplash boot splash screen...
[    4.209180] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    4.227178] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[    4.271895] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    4.304748] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    4.329192] cryptodev: loading out-of-tree module taints kernel.
[    4.334387] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network …ts from Kernel co[    4.344087] cryptodev: driver 1.12 loaded.
mmand line...
[    4.369975] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems...
[    4.395838] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[    4.402082] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    4.429344] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    4.447556] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    4.874069] systemd-journald[174]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /media/ram...
         Mounting /var/volatile...
[    5.143686] audit: type=1334 audit(1651167747.772:2): prog-id=5 op=LOAD
[    5.150417] audit: type=1334 audit(1651167747.776:3): prog-id=6 op=LOAD
         Starting Rule-based Manage…for Device Events and Files...
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[    5.758929] random: crng init done
[  OK  ] Finished Load/Save Random Seed.
[  OK  ] Found device /dev/ttyS2.
[  OK  ] Started Network Time Synchronizatio[    5.868328] mc: Linux media interface: v0.10
n.
[  OK  ] Reached target System Initialization.
[    5.911326] videodev: Linux video capture interface: v2.00
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
[    6.019674] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000
[    6.040004] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
[    6.045460] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
[    6.045590] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:11 UTC (11)
[    6.052555] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    6.055241] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
[    6.072572] systemd-journald[174]: Time jumped backwards, rotating.
[    6.081431] remoteproc remoteproc0: 5000000.m4fss is available
[  OK  ] Listening on dropbear.socket.
[    6.092516] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[    6.107350] remoteproc remoteproc0: powering up 5000000.m4fss
[    6.113591] remoteproc remoteproc0: Direct firmware load for am62-mcu-m4f0_0-fw failed with error -2
[    6.122882] platform 78000000.r5f: configured R5F for IPC-only mode
[    6.123079] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
[    6.129516] remoteproc remoteproc0: request_firmware failed: -2
[    6.137866] remoteproc remoteproc1: 78000000.r5f is available
[    6.151841] remoteproc remoteproc1: attaching to 78000000.r5f
[    6.158462] platform 78000000.r5f: R5F core initialized in IPC-only mode
[    6.165363] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node r5f-dma-memory@9da00000
         Starting D-Bus System Message Bus...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Reached target Socket Units.
[    6.283967] virtio_rpmsg_bus virtio0: rpmsg host is online
[    6.289678] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    6.301061] rproc-virtio rproc-virtio.1.auto: registered virtio0 (type 7)
[    6.308133] remoteproc remoteproc1: remote processor 78000000.r5f is now attached
[    6.312414] sii902x 1-003b: supply iovcc not found, using dummy regulator
[    6.361018] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
[    6.361104] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    6.427690] i2c i2c-1: Added multiplexed i2c bus 3
[    6.469881] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[    6.483032] tidss 30200000.dss: [drm] Cannot find any crtc or sizes
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Reached target Basic System.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[    6.764175] audit: type=1334 audit(12.216:4): prog-id=7 op=LOAD
[    6.770322] audit: type=1334 audit(12.220:5): prog-id=8 op=LOAD
         Starting User Login Management...
[  OK  ] Started TEE Supplicant.
         Starting telnetd.service...
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Started telnetd.service.
         Starting LSB: Expand Rootfs of boot device...
[  OK  ] Started User Login Management.
[  OK  ] Started LSB: Expand Rootfs of boot device.
[    7.453636] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    7.499841] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    7.506765] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    7.515552] cfg80211: failed to load regulatory.db
[  OK  ] Started Network Configuration.
[    7.672289] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
[    7.681712] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
         Starting Wait for Network to be Configured...
         Starting Network Name Resolution...
[    7.780202] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[    7.839887] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting containerd container runtime...
[  OK  ] Started Netperf Benchmark Server.
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Permit User Sessions...
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[    8.861828] remoteproc remoteproc2: 30074000.pru is available
[    8.868685] remoteproc remoteproc3: 30078000.pru is available
[    8.964925] tps6598x 0-003f: Unable to find the interrupt, switching to polling
[    9.088212] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
[  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[  OK  ] Reached target Hardware activated USB gadget.
[    9.229873] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    9.235795] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[    9.246950] xhci-hcd xhci-hcd.3.auto: USB3 root hub has no ports
[    9.253514] xhci-hcd xhci-hcd.3.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[    9.263074] xhci-hcd xhci-hcd.3.auto: irq 458, io mem 0x31100000
[    9.284977] hub 1-0:1.0: USB hub found
[    9.289147] hub 1-0:1.0: 1 port detected
         Starting Save/Restore Sound Card State...
[  OK  ] Finished Save/Restore Sound Card State.
[  OK  ] Created slice Slice /system/systemd-fsck.
[  OK  ] Reached target Sound Card.
[  OK  ] Found device /dev/mmcblk0p13.
         Starting File System Check on /dev/mmcblk0p13...
[  OK  ] Finished Synchronize System and HW clocks.
[  OK  ] Found device /dev/mmcblk0p1.
         Starting File System Check on /dev/mmcblk0p1...
[  OK  ] Finished File System Check on /dev/mmcblk0p13.
         Mounting /run/media/mnt/vendor/pers-mmcblk0p13...
[  OK  ] Finished File System Check on /dev/mmcblk0p1.
[    9.842772] EXT4-fs (mmcblk0p13): mounted filesystem with ordered data mode. Quota mode: none.
[  OK  ] Found device /dev/mmcblk0p12.
[  OK  ] Mounted /run/media/mnt/vendor/pers-mmcblk0p13.
         Mounting /run/media/bootloader-mmcblk0p1...
         Starting File System Check on /dev/mmcblk0p12...
[  OK  ] Mounted /run/media/bootloader-mmcblk0p1.
[  OK  ] Finished File System Check on /dev/mmcblk0p12.
         Mounting /run/media/metadata-mmcblk0p12...
[   10.045514] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Quota mode: none.
[  OK  ] Mounted /run/media/metadata-mmcblk0p12.
[  OK  ] Finished Print notice about GPLv3 packages.
[  OK  ] Found device /dev/mmcblk1p1.
         Starting File System Check on /dev/mmcblk1p1...
[  OK  ] Finished File System Check on /dev/mmcblk1p1.
         Mounting /run/media/BOOT-mmcblk1p1...
[  OK  ] Started containerd container runtime.
[  OK  ] Mounted /run/media/BOOT-mmcblk1p1.

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project am62xx-evm -

Arago 2023.04 am62xx-evm -

am62xx-evm login: root
[   16.220524] audit: type=1334 audit(21.672:6): prog-id=9 op=LOAD
[   16.226531] audit: type=1334 audit(21.676:7): prog-id=10 op=LOAD
[   16.549677] audit: type=1006 audit(22.000:8): pid=925 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[   16.561412] audit: type=1300 audit(22.000:8): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe9f7b268 a2=1 a3=ffffa05f7020 items=0 ppid=1 pid=925 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[   16.587001] audit: type=1327 audit(22.000:8): proctitle="(systemd)"
[   16.593324] audit: type=1334 audit(22.028:9): prog-id=11 op=LOAD
[   16.599387] audit: type=1300 audit(22.028:9): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffcf909100 a2=78 a3=0 items=0 ppid=1 pid=925 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[   16.624050] audit: type=1327 audit(22.028:9): proctitle="(systemd)"
[   16.630429] audit: type=1334 audit(22.040:10): prog-id=11 op=UNLOAD
[   16.636765] audit: type=1334 audit(22.040:11): prog-id=12 op=LOAD
root@am62xx-evm:~# 

  • Linux boot in the SDK is not optimized by default. For fastest boot times on AM62, you need to use OSPI NOR or EMMC boot modes and will also need to use Falcon boot mode. 

    DEtails of setting up Falcon boot mode on AM62 are described in here:

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1205638/faq-am625-how-to-boot-from-r5-u-boot-spl-directly-into-the-linux-kernel-skipping-a53-spl-and-a53-u-boot-falcon-mode

    there are several other steps that we have taken to get minial linux booted up with display and networking in <800 ms. This work is currently being intergrated in the SDK and will be available by 9.02 time frame by end of 1Q24. 

    Some of the steps are as below:

    1. Reduce Kernel size to only include modules required for application and build some drivers as modules and load after inital boot

    2. Use InitRAMFS for filesystem

    3. Lowest DDR init time is with single rank DDR

    4. If secure boot is needs use auth_type=2 with authentication APIs

    Hope this view helps.

    Thanks and Regards,

    Rahul 

  • Hi Rahul

    Can your team please provide with practical guidance / application note based on PSDK/Yocto code example which can be applicable to Sitara and Jacinto seires as many of customer wants to optimiza boot time?

    Also refer the similar content link from 3rd party SOM supplier. 

    U-Boot optimization

    • Remove the U-Boot splash screen on SOMs that support it.
      You can disable the splash screen using the U-Boot command line by following this example.
      To completely remove the splash screen support from your U-Boot you should also disable CONFIG_VIDEO in the U-Boot source code.
    • Change CONFIG_BOOTDELAY to 0 in U-Boot to save the second of delay before the autoboot occurs.
    • If your application requires an extremely fast boot, consider implementing Falcon mode for further time reduction – skipping U-Boot completely and loading the kernel from SPL.
      Note: make sure you are not skipping important code from the U-Boot board file. If needed, move such code from U-Boot to SPL.
      Read this guide to learn more about how to add support for Falcon Mode.
    • Append “quiet” to the kernel command line – it will quiet down the prints during boot, which takes time.

     

    Linux optimization

    • Remove unneeded drivers from the default kernel configuration to gain a slimmer and cleaner kernel image that can be loaded faster.
    • Remove or disable unneeded nodes from the device tree.
    • Build as modules required drivers that can be loaded at the end of the boot.

     

    Rootfs optimization

    • Remove from the filesystem unneeded packages that run on startup. Using Yocto, we recommend starting with core-image-minimal or core-image-base as a minimal image and adding to it only the packages you need.
    • If it makes sense for your application, you can consider running your filesystem from a RAM disk: this is sometimes used for small read-only filesystems.

    https://www.variscite.com/blog/how-to-reduce-boot-time/

    Thanks.

    Regards, 

    Jack

  • Jack Cha,

    Our plan is to integrate fast Linux boot example reference into the SDK by 9.2 time framer (March 2024). The E2E is one option but booting Linux using MCU+SDK provided bootloader is another option to parallelize boot. In 9.2, time frame we will have a Arago/yocto build configuration, user guide/app note for optimizing boot. Until then the only published resource is the falcon boot E2E FAQ which should get boot to < 3 seconds

     Regards,

    Rahul