This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62A: DCC debugging tool to debug related problems

Genius 13655 points

Part Number: PROCESSOR-SDK-AM62A

Hello Champs,

1.Auto Exposure
get_imx390_ae_dyn_params (IssAeDynamicParams * p_ae_dynPrms)
{
int32_t status = -1;
uint8_t count = 0;

g_return_val_if_fail (p_ae_dynPrms, status);

p_ae_dynPrms->targetBrightnessRange.min = 40;
p_ae_dynPrms->targetBrightnessRange.max = 50;
p_ae_dynPrms->targetBrightness = 45;

p_ae_dynPrms->threshold = 1;
p_ae_dynPrms->enableBlc = 1;
p_ae_dynPrms->exposureTimeStepSize = 1;

p_ae_dynPrms->exposureTimeRange[count].min = 100;
p_ae_dynPrms->exposureTimeRange[count].max = 33333;

p_ae_dynPrms->analogGainRange[count].min = 1024;
p_ae_dynPrms->analogGainRange[count].max = 8192;
p_ae_dynPrms->digitalGainRange[count].min = 256;
p_ae_dynPrms->digitalGainRange[count].max = 256;
count++;

p_ae_dynPrms->numAeDynParams = count;
status = 0;
return status;
}


Issue:
i、There is only one set of targetbrightness, is the targetbrightness the same in different time scenarios reasonable?
ii、If 60FPS is required, what should be the exposure time? How is the maximum and minimum exposure time determined?
2.Color depth supported by DCC

Issue:
i、DCC userguide Only the raw10 and raw12 images can be used for debugging?
ii、The current DCC tuning tool color depth can be selected 10/12/14/16bits per pixel, is 14/16bit raw image can also be used for debugging?



Thanks
Regards
Shine

  • Hi Shine,

    There is only one set of targetbrightness, is the targetbrightness the same in different time scenarios reasonable?

    To set the target brightness range:

    • [targetBrightness - threshold, targetBrightness + threshold]
    If 60FPS is required, what should be the exposure time? How is the maximum and minimum exposure time determined?

    You may refer to the driver source code for the minimum and maximum exposure time.

    DCC userguide Only the raw10 and raw12 images can be used for debugging?

    I am not very familiar in using the tool to debug, do you have any comments on this?

  • i、There is only one set of targetbrightness, is the targetbrightness the same in different time scenarios reasonable?

    For real applications, AE target could possibly vary, but that seems rare as far as I know.

    ii、If 60FPS is required, what should be the exposure time? How is the maximum and minimum exposure time determined?

    It depends on the application requirements and sensor.
    For 60fps, the maximum exposure time can be up to 16.66ms.

    i、DCC userguide Only the raw10 and raw12 images can be used for debugging?
    ii、The current DCC tuning tool color depth can be selected 10/12/14/16bits per pixel, is 14/16bit raw image can also be used for debugging?

    I am not sure what you mean by debugging here.

    Most tuning tool plugins may support up to 16-bit input raw images.

  • Hi Le&Hua,

    Thank you very much for your great support.

    For the problem of Color depth, For example, when using 16bit raw plug_ins AWB operation, A pop-up window prompts:

    “WARNING:This image is overexposed.You may get wrong tuning valuss.Consider discarding this image and capturing it again with different setting.



    Thanks
    Regards
    Shine

  • when using 16bit raw plug_ins AWB operation,

    Are your 16-bit raw images coming output your sensor directly?

    Is your sensor output in 16-bit linear format to AM62A?

  • I am very sorry for not replying to you for a long time, because there are some problems with my account login.

    I have solved the error problem, because I use 16bit wdr raw, and the sensor directly produces 12bit linear raw.

    Thanks

  • Thanks for the update and we will close this thread!