Other Parts Discussed in Thread: DM3730
i am using the DM3730 EVM board from mistral...i need to learn from the basics..so i just start compling....
first i have complied the x-loader 1.46 psp 3.00.01.06
it shows 2 errors...
and then i have compled the u boot-2009-11
it shows some errors...the ECC something...i just add the one dit define error..
then it complied.....
there is no signGP in the host tools i thinking its missing...
and now i have complied the kernel linux 2.6.32
after all it shows
CHK include/linux/compile.h
Kernel: arch/arm/boot/Image is ready
Kernel: arch/arm/boot/zImage is ready
UIMAGE arch/arm/boot/uImage
"mkimage" command not found - U-Boot images will not be built
Image arch/arm/boot/uImage is ready
someone help me it will be the time saver for our project...
plz help us we are running out of time...