Here comes a question that is it the USB disconnection envelope detector threshold in AM3358 platform? Normally it is 400mV voltage amplitude in USB 2.0 data line, and the threshold in USB2.0 spec should be during 525mV~625mV, so we would like to learn if it is the precise threshold spec to define this in AM3358.
In my understanding, this HS_Disconnect threshold is in chip side and used to detect if DP/DN amplitude is over threshold or not, and the chip should disconnect the USB data communication as it is over threshold.
So, we would also like to know if it is the case that it is the higher driving current in device and might have the signal amplitude over the threshold and cause USB disconnection issue.