This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721EXCP01EVM

  • A little bit of looking at schematics shows that the two lights that are out on the Main Processor board are indications of VSYS_IO_3V3 and VSYS_MCUIO_3V3 which are generated from load switches U6 and U22 on the SOM.

    U6 generates VDD_IO_3V3_LS from VSYS_3V3 and EN_3V3IO_LDSW; EN_3V3IO_LDSW is the output of GPIO11 for PMIC-B; VDD_IO_3V3_LS directly becomes VSYS_IO_3V3.

    U22 generates VDD_MCUIO_3V3_LS from VCCA_3V3 (derived from VSYS_3V3) and EN_MCU3V3_LDSW; EN_MCU3V3_LDSW is the output of GPIO3 for PMIC-A; VDD_MCUIO_3V3_LS directly becomes VSYS_MCUIO_3V3.

    ---------

    The remaining LED that is lighted is powered by VSYS_3V3.

    A couple of ideas: 

    TP128 is a spot to measure VCCA_3V3; it is the input voltage to the PMICs; if this was not at the right level, then the board would behave as you are describing. VCCA_3V3 is shut off if VSYS_3V3 is too high. So, in case TP128 shows an incorrect voltage, check VSYS_3V3 at TP1.

    Did you write to either PMIC?