This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Parameter Consulting

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH

Hello,

We need the following SOC power supply parameters and power consumption

TDA4VH

Power network name

vmin vtyp vmax Imin Ityp Imax w功耗
SOC MAIN PROCESSOR

VDD_CPU_AVS*

VDD_RAM_0V85
VDD_CORE_0V8
VDD_DDR_1V1
VDD_WK_0V8
MAIN ANALOG VDD_PHY_1V8
VDD_CORE_0V8
VDA_DLL_0V8
VDA_PLL_1V8
VDDA_3P3_USB
MAIN DIGITAL VDD_IO_3V3
VDD_GPIORET_3V3
VDD_SD_DV**
VDD_VDDIO_1V8
VDD_EFUSE_1V8
MCU MCU SAFETY ISLAND VDA_MCU_1V8
VDD_MCU_0V85
VDD_MCUGPIOET_3V3
VDD_MCUIO_1V8
VDD_MCUIO_3V3
VDD_MCUWK_0V8

Regards,

Gary

  • The following 2 tables show the power per rail for our Superset use case; this use case is a heavy loading.
    The first table is a thermal power and the second table is a PDN power.

    Thermal Power not suitable for designing a PDN
      Total Power [mW] Voltage [V]
    VDD_CORE 14480 0.8
    VDD_CPU 23420 0.76
    VDD_MCU 780 0.8
    VDDAR_CORE 460 0.85
    VDDAR_CPU 890 0.85
    VDDAR_MCU 52 0.85
     
    VDD_WAKE0 10 0.8
    VDD_MCU_WAKE1 10 0.8
     
    VDDS_DDR 681 1.1
    VDDS_DDR_C0 0 1.1
    VDDS_DDR_C1 0 1.1
    VDDS_DDR_C2 0 1.1
    VDDS_DDR_C3 0 1.1
    VDDA_0P8_PLL_DDR0 8 0.8
    VDDA_0P8_PLL_DDR1 8 0.8
    VDDA_0P8_PLL_DDR2 8 0.8
    VDDA_0P8_PLL_DDR3 8 0.8
     
    VDDA_1P8_CSIRX0_1 54 1.8
    VDDA_1P8_CSIRX2 27 1.8
    VDDA_0P8_CSIRX0_1 39 0.8
    VDDA_0P8_CSIRX2 22 0.8
     
    VDDA_1P8_DSITX 6 1.8
    VDDA_0P8_DSITX 42 0.8
    VDDA_0P8_DSITX_C 13 0.8
     
    VDDA_1P8_SERDES0_1 240 1.8
    VDDA_1P8_SERDES2 130 1.8
    VDDA_1P8_SERDES4 130 1.8
    VDDA_1P8_SERDES2_4 5 1.8
    VDDA_0P8_SERDES0_1 265 0.8
    VDDA_0P8_SERDES2 135 0.8
    VDDA_0P8_SERDES4 125 0.8
    VDDA_0P8_SERDES_C0_1 32 0.8
    VDDA_0P8_SERDES_C2 14 0.8
    VDDA_0P8_SERDES_C4 24 0.8
     
    VDDA_3P3_USB 2 3.3
    VDDA_1P8_USB 1 1.8
    VDDA_0P8_USB 6 0.8
     
    VDDA_1P8_UFS 4 1.8
    VDDA_0P8_UFS 7 0.8
     
    VDDS_MMC0 100 1.8
    VDDA_0P8_DLL_MMC0 6 0.8
     
    VDDA_ADC0 7 1.8
    VDDA_ADC1 7 1.8
     
    VDDA_MCU_PLLGRP0 22 1.8
     
    VDDA_PLLGRP0 8 1.8
    VDDA_PLLGRP1 22 1.8
    VDDA_PLLGRP2 14 1.8
    VDDA_PLLGRP5 8 1.8
    VDDA_PLLGRP6 14 1.8
    VDDA_PLLGRP7 16 1.8
    VDDA_PLLGRP8 16 1.8
    VDDA_PLLGRP9 8 1.8
    VDDA_PLLGRP10 14 1.8
    VDDA_PLLGRP12 20 1.8
    VDDA_PLLGRP13 6 1.8
     
    VDDA_MCU_TEMP 7 1.8
     
    VDDA_TEMP0 3 1.8
    VDDA_TEMP1 3 1.8
    VDDA_TEMP2 3 1.8
    VDDA_TEMP3 3 1.8
    VDDA_TEMP4 3 1.8
     
    VDDA_WKUP 7 1.8
    VDDA_POR_WKUP 3 1.8
    VDDA_OSC1 7 1.8
     
    VDDSHV3P3_MCU 157 3.3
    VDDSHV1P8_MCU 12 1.8
     
    VDDSHV3P3 313 3.3
    VDDSHV1P8 9 1.8

    PDN (Peak) Power Peak power is intended for PDN resourcing
      Total Power [mW] Voltage [V]
    VDD_CORE 19230 0.8
    VDD_CPU 35500 0.76
    VDD_MCU 1020 0.8
    VDDAR_CORE 550 0.85
    VDDAR_CPU 1070 0.85
    VDDAR_MCU 62 0.85
     
    VDD_WAKE0 10 0.8
    VDD_MCU_WAKE1 10 0.8
     
    VDDS_DDR 1211 1.1
    VDDS_DDR_C0 0 1.1
    VDDS_DDR_C1 0 1.1
    VDDS_DDR_C2 0 1.1
    VDDS_DDR_C3 0 1.1
    VDDA_0P8_PLL_DDR0 8 0.8
    VDDA_0P8_PLL_DDR1 8 0.8
    VDDA_0P8_PLL_DDR2 8 0.8
    VDDA_0P8_PLL_DDR3 8 0.8
     
    VDDA_1P8_CSIRX0_1 59 1.8
    VDDA_1P8_CSIRX2 30 1.8
    VDDA_0P8_CSIRX0_1 42 0.8
    VDDA_0P8_CSIRX2 24 0.8
     
    VDDA_1P8_DSITX 6 1.8
    VDDA_0P8_DSITX 46 0.8
    VDDA_0P8_DSITX_C 14 0.8
     
    VDDA_1P8_SERDES0_1 260 1.8
    VDDA_1P8_SERDES2 140 1.8
    VDDA_1P8_SERDES4 140 1.8
    VDDA_1P8_SERDES2_4 5 1.8
    VDDA_0P8_SERDES0_1 295 0.8
    VDDA_0P8_SERDES2 145 0.8
    VDDA_0P8_SERDES4 135 0.8
    VDDA_0P8_SERDES_C0_1 35 0.8
    VDDA_0P8_SERDES_C2 14 0.8
    VDDA_0P8_SERDES_C4 26 0.8
     
    VDDA_3P3_USB 2 3.3
    VDDA_1P8_USB 1 1.8
    VDDA_0P8_USB 6 0.8
     
    VDDA_1P8_UFS 4 1.8
    VDDA_0P8_UFS 7 0.8
     
    VDDS_MMC0 110 1.8
    VDDA_0P8_DLL_MMC0 7 0.8
     
    VDDA_ADC0 8 1.8
    VDDA_ADC1 8 1.8
     
    VDDA_MCU_PLLGRP0 24 1.8
     
    VDDA_PLLGRP0 8 1.8
    VDDA_PLLGRP1 24 1.8
    VDDA_PLLGRP2 15 1.8
    VDDA_PLLGRP5 8 1.8
    VDDA_PLLGRP6 15 1.8
    VDDA_PLLGRP7 18 1.8
    VDDA_PLLGRP8 18 1.8
    VDDA_PLLGRP9 8 1.8
    VDDA_PLLGRP10 15 1.8
    VDDA_PLLGRP12 22 1.8
    VDDA_PLLGRP13 7 1.8
     
    VDDA_MCU_TEMP 7 1.8
     
    VDDA_TEMP0 4 1.8
    VDDA_TEMP1 4 1.8
    VDDA_TEMP2 4 1.8
    VDDA_TEMP3 4 1.8
    VDDA_TEMP4 4 1.8
     
    VDDA_WKUP 8 1.8
    VDDA_POR_WKUP 4 1.8
    VDDA_OSC1 8 1.8
     
    VDDSHV3P3_MCU 180 3.3
    VDDSHV1P8_MCU 14 1.8
     
    VDDSHV3P3 345 3.3
    VDDSHV1P8 11 1.8
     
    VPP_MCU 720 1.8
    VPP_CORE 720 1.8