Part Number: AM62A7-Q1
We use the chip AM62A74AUMHAAMBR, does it mean we can use either 0.75V or 0.85V for the VDD_CORE, the mainly difference between them is running speed?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello zenanding
Thank you for the query.
Please refer below the OPP for the device based on the selected part number.


We use the chip AM62A74AUMHAAMBR, does it mean we can use either 0.75V or 0.85V for the VDD_CORE, the mainly difference between them is running speed?
The SoC can operate at 0.75 or 0.85V. Note that VDD_CORE cannot be scaled dynamically.
The provision is provided in the PMIC to be able to configure the VDD_CORE voltage using a GPIO.
regards,
Sreenivasa
OK, thanks. As we don't connect the GPIO6 OUT(it's float now), we will use the SOC vdd_core by default 0.75V
Hello zenanding,
Thank you.
As we don't connect the GPIO6 OUT(it's float now), we will use the SOC vdd_core by default 0.75V
This is correct. the recommendation is for future expansion.
Regards,
Sreenivasa
Hello zenanding,
I will close the thread if you do not have additional queries.
Regards,
Sreenivasa