This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: Power consumption and Ethernet interface CPSW3G CPPI

Part Number: AM62A7

Hi, 

Q1. There is less information regarding the power consumption of AM62Ax compared to AM62x. Do you have any information you can provide? I was able to find the following documentation.
https://www.ti.com/lit/an/sprad93/sprad93.pdf

Also, do you have any advice or materials for designing with low consumption such as deep sleep? We plan to use the following peripherals.
・EMMC
・MIPI
・DSI
・I2C/SPI/UART

Q2. According to the data sheet, it says that the external Ethernet port is 2 ports and the internal port is 1. What does that mean?

Thanks,

Conor