Hi,
Now i have modified the demo on encoder on dm365 evm.Now for the project uitility, i have removed some input modules remainning the TVP5150 from the board,and connected the tvp5150 with the main chip(dm365) directly.But how could i do to remove the relative drivers from the kernel.Now i have disabled the tvp7002 driver in the dm365 menuconfig, but how to modify other relative source code.Another, what is the input method via tvp5150?? Is it ' Capture_Input_COMPOSITE '??
Regards