Part Number: DRA821U
How can I build the example below that is described on this page?
|
Example |
Application Name |
Description |
Cores Supported |
|---|---|---|---|
|
FreeRTOS Task Switch |
freertos_test_task_switch |
The FreeRTOS Task Switch Example test performs the following:
1. switch between ping and pong tasks using semaphores
2. switch between ping and pong tasks using direct-to-task notifications
3. switch from ping task to ISR to pong task and back to ping task using semaphores, here there is a task switch
|
mcu1_0, mcu1_1, mcu2_0, mcu2_1 |
I have tried this
make -s all BOARD=j7200_evm BUILD_PROFILE=debug CORE=mcu2_0
That builds several .xer5f files but nothing with FreeRTOS. Most of the .xer5f images are release, so no symbols. There are only a couple of debug images that get built, but its an odd collection, these are the only debug images built.
- csl_i2c_led_blink_app_mcu1_0_debug.xer5f
- csl_mailbox_sender_receiver_app_mcu1_0_debug.xer5f
- ocmc_memory_benchmarking_app_freertos_mcu2_0_debug.xer5f (this is named debug, but there are no symbols)
There is a build error,
/bin/sh: 1: mono: not found
That seems to be related to SBL builds, if you can point me to where to get mono that would help too.
Thanks
Jeff
Jeff