Part Number: TMDXIDK5718
Hi,
I would like to install podman on my sdk image, is this possible? If so, how is it possible to do it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDXIDK5718
Hi,
I would like to install podman on my sdk image, is this possible? If so, how is it possible to do it?
Hi Jafet,
This can be done through building a custom Yocto image. A forewarning however, since podman and docker are not supported for the AM57, I can't offer extensive support if podman requires debugging.
To build and install podman onto your SDK image, you'll have to create a custom image recipe that includes the podman-compose recipe. Thankfully, podman already comes built into the meta-virtualization layer so you won't have to install anything from source to get this to work.
These two links should be helpful:
To test whether podman will work without going through the process of creating a custom image, you can build and install the package by itself.
Build the package by running:
TOOLCHAIN_BASE=<path-to-toolchain> MACHINE=am57xx-evm bitbake -k podman-compose
Then install the generated .ipk file:
# find the .ipk file$ find -name *podman-compose*.ipk# transfer the file to the target with scp, sftp, etc.
# install the package (run this on target)
$ opkg -V2 install <ipk-file-name>
Best,
Jared