This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Advice on C6713 solution

I am trying to design a C6713 DSK prototype to demonstrate the performance gains in upgrading an existing system.

Specification:

4 Simultaneously sampled channels at 10MHz - any suggestions for daughter cards?

The processing generates 600kB/s worth of data which ideally needs to be displayed on the host PC. - I know this data rate is unreasonable for RTDX (which is no longer supported). So lets assume some level of threshold to reduce this data, what other methods can be used?

For example, can anyone recommend a C6713 based PCI card? If so, can these come with analogue front ends for 10MHz?

Any advice would be really great, thanks,

James.