This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: ICSSG Ethernet driver - SRAM details

Part Number: AM6442

Dear TI team,

I was checking the Processor SDK user manual regarding the ICSSG ethernet usage i have seen some SRAM requirements as shown below.

3.6.3.4.10. SRAM Requirement

  • The ICSSG Ethernet driver can be used in switch mode. Two icssg ports are used per switch.
  • SRAM Required for each switch (per two ports) is 256 KB.
  • For each ICSSG switch, the SRAM required needs to be contiguous.
  • PRUETH only uses the required amount of SRAM from the SRAM/MSMC pool. If PRUETH doesn’t get the required amount of SRAM, the prueth_probe() API will return with -ENOMEM error.