This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error: unrecognized/unsupported machine ID (r1 = 0x00000ca4).

Other Parts Discussed in Thread: AM3517

Hi

i'm using a phyCORE-AM35xx Board with AM3517 microprocessor and i want to install Android on it.

i downloaded the TI_Android_DevKit 2.2 and 2.3 and i followed the instructions in the user guide, preparing and sd card with android on it and trying to boot from sd card.

when i use the android 2.3, the u-boot says that the kernel loaded successfully but the board hangs.

when i use the android 2.2, the kernel loads but displays the error: "Error: unrecognized/unsupported machine ID (r1 = 0x00000ca4)."

the following is the captured output of the board on serial port.

 

U-Boot 2009.11 (Apr 22 2011 - 14:43:05)

OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz
phyCORE-AM35xx Board + LPDDR/NAND
I2C:   ready
DRAM:  256 MB
NAND:  256 MiB
In:    serial
Out:   serial
Err:   serial
Die ID #2f1e0001000000000158b6b402011012
Net:   davinci_emac_initialize
Ethernet PHY: GENERIC @ 0x00
DaVinci EMAC
Hit any key to stop autoboot:  0
PCM048 # mmc init
mmc1 is available
PCM048 # fatload mmc 0 0x82000000 boot.scr
reading boot.scr

417 bytes read
PCM048 # source 0x82000000
## Executing script at 82000000
reading uImage

2563824 bytes read
***** Kernel: /dev/mmcblk0p1/uImage *****
***** RootFS: /dev/mmcblk0p2 *****
## Booting kernel from Legacy Image at 80200000 ...
   Image Name:   Linux-2.6.32
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2563760 Bytes =  2.4 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux............................................................................................................................................................... done, booting the kernel.

Error: unrecognized/unsupported machine ID (r1 = 0x00000ca4).

Available machine support:

ID (hex)        NAME
00000898        OMAP3517/AM3517 EVM

Please check your kernel config and/or bootloader.